Skip to main content
AlexSmart
Associate III
August 25, 2020
Solved

STM32H7 + Keil + CubeMX?

  • August 25, 2020
  • 2 replies
  • 1707 views

Getting started with STM32H7, faced a problem.

Ive worked for a long time with STM32F4 in Keil uVision (version 5.24.2.0), used a "classic" option, configuration via RTE_Device.h. Worked perfect.

Now I dont have such option with STM32H7, only CubeMX, and adventures began.

Created project with CubeMX, project building successfully. But when Im trying to add something i.e. filesystem, rtos, etc, it says that it is necessary to start CubeMX (again), and it starts complete different CubeMX project, a new one. Ok, fine, It adds a new main.c, stm32h7xx_it.c, etc. Obviously fails to build.

Creating project with Keil looks makes a bit more sense, but still unable to build up a complete application, got the same issue as

https://community.st.com/s/question/0D50X00009kHvWr/keil-mdk-and-st32cubemx-not-interacting

Is there a way to not use CubeMX in any way?

This topic has been closed for replies.
Best answer by AlexSmart

Updating Keil uVision to V5.31.0.0 worked

2 replies

Tesla DeLorean
Guru
August 25, 2020

Can use the H7 HAL directly, should be MDK projects and templates in the example trees.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
AlexSmart
AlexSmartAuthorBest answer
Associate III
August 26, 2020

Updating Keil uVision to V5.31.0.0 worked