User Activity

I have interesting problem.Custom PCB as master role using SDK 1.15.0.Trying bonding procedure, I find an situatiotion where after ACI_GAP_PAIRING_COMPLETE_VSEVT_CODE event, waiting 100ms (as in "BLE_HeartRateFreeRTOS_ANCS" example) (Ithink it is a m...
2 years ago it happened that the controller turned to brick. I corresponded with technical support for a long time and I was offered to send the controller to the factory or representative. But since the case was a single one, I did not take advantag...
Hi!I cannot change Application Structure from "Basic" to "Advanced". Same posts (post1, post2 ) did not solve the problem.
Hi.Using STM32Cubeprogrammer API v.2.7.0 with STM32WB55 and USB interface, I find an error when to call initOptionBytesInterface()....peripheral_C* options_bytes;options_bytes = initOptionBytesInterface();...As we know, "peripheral_C" structure have ...
Hi.I want to write desktop application using STM32CubeProgrammer API to load FUS and stack to STM32WB. But in documentation I can`t find any mentioning about how to start FUS, update FUS and load stack.Or does the API do not give this opportunity?
Kudos from