STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1568 Views
  • 0 replies
  • 2 kudos

Resolved! STM32H723 Pinout PC2_C/PC3_C

Hello everybody!The documentation indicates that this leg can only be configured as an ADC input. In "CUBE MX" it can be defined as different kinds of interfaces. Who should I believe that my project would work properly and I would not be faced with ...

0693W000007BWxFQAW.png 0693W000007BWxKQAW.png 0693W000007BWxPQAW.png
AB.19 by Associate II
  • 2710 Views
  • 2 replies
  • 0 kudos

Resolved! Can't create MDK-ARM project for STM32L011F4U

Cube version: 6.1.1Java: Oracle SE 15.0.2 (64bit)Toolchain: MDK-ARM V5Part: STM32L011F4UWhen I create an empty project and press generate, the generation fails. First I get a empty dialog screen:And then an error:Is this a bug?

0693W000007Du3eQAC.png 0693W000007Du4NQAS.png
allard by Senior
  • 1190 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CubeIDE bug or not?

I use STM32CubeIDE under MacOS. I don't understand whether it is a bug or not. I can not change Input frequency of HSE in clock configuration. I can do it in CubeMX under Window on the same project.

0693W000007DJGlQAO.png
EL314 by Associate III
  • 1471 Views
  • 2 replies
  • 0 kudos

Enabling Ethernet Interface on Nucleo-H743ZI2

Hi,I am developing a TCP/IP server for my application on the Nucleo-H743ZI2 board. I want to use LWIP with FreeRTOS to allow threading and have a similar syntax to POSIX sockets.So far I found the following two examples:(1) This tutorial targets the ...

0693W000007CsFWQA0.png 0693W000007CsJJQA0.png 0693W000007CsIWQA0.png 0693W000007CsJxQAK.png
HA87 by Associate III
  • 8484 Views
  • 8 replies
  • 1 kudos

Resolved! MII on STM32H730VBTx

STM32CubeMX doesn't show MII as an option for Ethernet on the STM32H730VBTx. Is MII not available on this part (RMII only?) or is there a problem with STM32CubeMX? The datasheet suggests it should support MII.

Aasdf.3 by Associate
  • 1583 Views
  • 2 replies
  • 0 kudos