STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1547 Views
  • 0 replies
  • 2 kudos

Resolved! Disable Resolve Clock Issues

Hi there!Is there a way to permanently disable the resolve clock issues feature of STM32CubeIDE-1.7.0? I've tried saying "No" and remember my options, but the interface just completely ignores me and does it anyway. It's utterly infuriating. Is there...

etheory by Senior II
  • 3618 Views
  • 6 replies
  • 0 kudos

Can G491 OPAMP6 be connected to ADC3?

In RM0440, STM32G491 is Category 4.Therefore OPAMP6 can be connected to ADC3 refer to RM0440 21.4.4(ADC Connectivity)But I cannot find check option for OPAMP6 in ADC3 setting.Is it unavailable? or not implemented yet?

0693W000008xSTkQAM.png
yjsbd by Associate II
  • 2152 Views
  • 4 replies
  • 0 kudos

STM32H7 - SDMMC/SDIO not working, wrong Signal-Levels

Hi,I have a similar issue like this:https://community.st.com/s/question/0D50X00009XkWtOSAV/stm32h7-sdmmc-not-workingHost: "Nucleo-STM32H743"Target-Interface: SDIO V2.0 Clk = 12 MHz (Silabs WFM200S)-error pattern:At "read_cmd53" the 3V3-Signallevel br...

0693W00000Dn7BQQAZ.png 0693W00000Dn7D7QAJ.png
TTimm.1 by Associate II
  • 2706 Views
  • 4 replies
  • 0 kudos

1) What is the latest CMSIS version 5 support for STM32F7 and where can i find it. 2)Also any other methods and mechanisms to perform optimizations for floating-point operations in the given STM32F7 MCU platform.

Currently our customer implemented intensive mathematical floating-point double-precision algorithms in Matlab and converted them into C code using the Matlab Code Conversion tool. He needs to perform further platform-level optimizations using CMSIS ...

PGama by Associate II
  • 1557 Views
  • 1 replies
  • 0 kudos

USB-DFU example bug (STM32H7)

I am showing that USB-DFU example available in latest CubeMX STM32Cube_FW_H7_V1.9.0 package (/Projects/NUCLEO-H7A3ZI-Q/Applications/USB_Device/DFU_Standalone) does not work. The example contains this code:/* Test if user code is programmed starting f...

TDJ by Lead
  • 2185 Views
  • 3 replies
  • 1 kudos