STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1568 Views
  • 0 replies
  • 2 kudos

Hi, i am working on STM32L073 controller. I am using USB interface to communicate between host (docklight in my case) and controller. I am facing issue related to endianness here.

following packet i am sending from host to controller-02 01 00 02 01 02 03 04 00 01 00(first two bytes are packet type)-controller is expecting that value as 0x0102 but due to endianness mismatch when sent as 0x0102 its interpreted as 0x0201.so every...

BChav.1 by Associate III
  • 1330 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H735G-DK ADC accuracy

Hello. I'm using the STM32H735G-DK and I run into a problem when using the ADC, so I made a very short CubeMX project to check this.I started with a CubeMX configured board with no peripheral default initialisation.Then I ticked ADC1 IN0. So by defau...

akbjk.1 by Associate II
  • 2056 Views
  • 3 replies
  • 0 kudos

Unable to debug unmanaged makefile project

We have a project created in CubeMX (inside CubeIDE) and developed in CubeIDE. Everything works fine.However, we wanted to use a Makefile so we could have the same build process on our CI server and within CubeIDE.So we now generated a Makefile from ...

FS.1 by Associate III
  • 3589 Views
  • 5 replies
  • 0 kudos

I2C2 conflict with CAN2

Hello, I am going to use CAN1, CAN2 and I2C1, I2C2. As the attached picture shows, the I2C2 has a conflict with CAN2. IS there any way to fix it? I have to use both CAN modules and two I2C's. Thank you.

NASI by Senior
  • 1710 Views
  • 3 replies
  • 0 kudos

STM32CubeMX version 4.7.0

Hi everyone. I'm facing some issues trying to open a project created in CubeMX version 4.7.0. Once the project was not created by me, I don't want to migrate it to a newer version (and if I do, which I had already done, I get some errors in some of t...

Nucleo-H743ZI Ethernet Communication

I am working on getting a Nucleo-H743ZI2 board to communicate with a python GUI over Ethernet. I am using CubeMX to initialize all of my peripherals and CubeIDE for development. For testing I have used the Lwip_HTTP_Server_Netconn_RTOS for STM32H743Z...

0693W00000DnaBUQAZ.png 0693W00000DnaBoQAJ.png 0693W00000DnaByQAJ.png 0693W00000DnaGeQAJ.png
MAgui.1 by Associate II
  • 3103 Views
  • 2 replies
  • 0 kudos

Question about debugging in sw4stm32

I use STM32F429ZI​ with dwm3000evb from decawave I executed a example code in systemworkbench for stm32But there is an error message​info : unable to match requested speed 2000 khz, using 1800 khz​ I​ don't know how to solve this error and I want to ...

DCha.1 by Associate
  • 1306 Views
  • 1 replies
  • 1 kudos

startup_stm32f407xx.s ARMCLANG 6.x problem

Hi,i'm using Keil with the ARMClang 6.x compiler, an STM32f407 and CubeMX to configure my project.I was playing arround with dynamic memory allocation and was wondering whyuint8_t* b_; b_ = static_cast<uint8_t*>(std::calloc(100, sizeof(uint8_t)));wor...

Jnevi.1 by Senior
  • 2327 Views
  • 3 replies
  • 0 kudos