STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1589 Views
  • 0 replies
  • 2 kudos

Resolved! CAN: Clock Frequency Scaling Issues to Achieve Baud Rate

Hello,I am attempting to add CAN communication to one of my co-worker's boards, who is using the STM32F303RE MCU with an external 30 MHz crystal oscillator. The CAN communication uses the APB1 Peripheral Clock, which is currently using 30 MHz as well...

0693W00000YAiO3QAL.png
KMew by Senior III
  • 2177 Views
  • 3 replies
  • 1 kudos

Resolved! Why does CubeMX for the STM32H743i_EVAL board put the cart before the horse and completely ignore the BSP code when the SDMMCx is enabled?

Creating the project with CubeMX for the STM32H743i_EVAL board and allowing it to generate the Initializing function and call for the SDMMC1 (or 2 for that matter), generates initialization code that attempts to power up the card without checking to ...

Code is getting stuck at SystemClock_Config() function

Hello,I'm using STM32H747XIH6 MCU and I have developed the code on STM32 cube ide software 1.7.0 by generating the code in stm32 cube mx 6.5.0.I have written a simple code of GPIO toggle pin.Below is my code for clock configuration. I have connected ...

Aarra.1 by Senior
  • 4740 Views
  • 3 replies
  • 0 kudos

STM32CubeMX for STM32: Is it possible to use/set a Prefix or namespace for all functions/global variables generated by STMCubeMX C-Code Generator?

Reason for the question:We want to generate two different hardware settings (CubeMX projects) into one software program running on a STM32 controller. Then at startup, the controller finds out, which HW configuration it has to use and uses just one o...

Resolved! Timer - Conflict between ETR1 and Output Compare on CH1?

Hi,I've just tried to set up TIM2 on an STM32G0B1RE in CubeMX like this:The exact purpose shouldn't matter for this question, but the timer is supposed to generate an interrupt when a LOW pulse of a given minimum length is detected on an external sig...

0693W00000YACWKQA5.png

Resolved! I have used CubeMX to configure some GPIO pins for an interface to some other I/O devices. CubeMX generates initialization code for some other GPIO pins in gpio.c and main.h, but nothing for the I/O I defined.

I'm working on a project using a STM32H747XIHx dual core processor.  I believe I have the latest STM32CubeIDE and STM32CubeMX tools.  How do I configure CubeMX to generate GPIO initialization code for my I/O signals?

RGate.2 by Associate II
  • 4198 Views
  • 4 replies
  • 0 kudos

How to use usb hs in stm32f407zgt6 using usb3300?

The usb fs works fine for me, but when I try the usb hs, it gives me error_handler(). I don't know how I have to put it to make it work.My configuration:I use stm32cubeide.I don't know if my configuration is correct respect to pull up and pull down, ...

0693W00000Y7zayQAB.png 0693W00000Y7zbwQAB.png 0693W00000Y7zcaQAB.png 0693W00000Y7zd9QAB.png
IOR.1 by Associate
  • 2121 Views
  • 1 replies
  • 0 kudos