STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1557 Views
  • 0 replies
  • 2 kudos

How to set the desired clock frequency(SCL) for Nucleo-f401RE (Master-Receive- Half Duplex I2S Communication with MEMS Microhone - CUI Device (Slave) ).

Hello , I am using STM Cube IDE for I2S communication between NUCLEO-F401RE and CUI MEMS microphone namely CMM-4030DT-26354-TR . I am current facing a problem to set a clock frequency for SCL pin of Nucleo board. The SCL clock frequency range for ...

smit1 by Associate
  • 3743 Views
  • 2 replies
  • 0 kudos

I'm trying to generate code for a STM32U558 USB device The USB initialization function MX_USB_Device_Init is empty

STM32CubeMx version 6.7.0STM32Cube_FW_U5_V1.1.1STM32Cube_FW_U5_V1.1.1\Projects\B-U585I-IOT02A\Applications\USBX\Ux_Device_HID_CDC_ACM\Ux_Device_HID_CDC_ACM.iocCopying the ioc file to a new location, double clicking and clicking "generate code" shows ...

Inbara by Associate II
  • 2971 Views
  • 6 replies
  • 0 kudos

Resolved! How to set PB 8 as BOOT0 pin and PG10 as NRST pin

This is really a basic question, but nevertheless I haven't found an answer.I am confused primarily about visualization of PB8 and PG10 pins inside CubeIDE MX.When I create new project I would expect PB8 and PG10 looking "yellow" and also being defin...

0693W00000YA8BIQA1.png 0693W00000YA8AtQAL.png
GHrib.1 by Associate III
  • 3512 Views
  • 2 replies
  • 1 kudos

DMA fails with IRAM1/IRAM2 settings

Hi, I am trying to use SDIO with DMA and TIM1 PWM with DMA on STM32F407VETx.After generating code with STM32CubeMX v6.6.1 I get these settings:with these settings SDIO with DMA works, but TIM1 PWM with DMA fails.After an update generating code with S...

0693W00000Y8qzDQAR.png 0693W00000Y8qzDQAR.png
JBond.1 by Senior
  • 2262 Views
  • 5 replies
  • 0 kudos

Resolved! STM32G030K6T6 with only 8 ADCs

I am developing a STM32 project with STM32G030K6T6 ADC channels but when I start setting the MCU, it allows only 8 ADC convertions (the datasheet describes there are 12 and the system configuration allows to add up to 12 channels) . However, I need a...