STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1592 Views
  • 0 replies
  • 2 kudos

Resolved! SPI DMA configuration generated by STM32CubeMX does not work

I have used STM32CubeMX to generate the configuration required to use SPI1 with DMA for a nucleo H743ZI2 board:  Then, I generate the code as a Makefile project and modify the main function to have:int main(void) { /* USER CODE BEGIN 1 */   /* US...

0693W00000YASP6QAP.png 0693W00000YASaSQAX.png
DGast.1 by Associate III
  • 5132 Views
  • 7 replies
  • 1 kudos

Resolved! I cant seem to make a pwm work.

I have a project where I want to add a simple PWM. I'm using the stm32h series. I have a scope on PA3, and I set up my timer2 for PWM on channel 4. I did this all in the IOC file as I want to understand how to create the PWM I need. I see it added my...

ulao by Associate III
  • 3815 Views
  • 7 replies
  • 1 kudos

STM32F769I EVAL CAN problems

Hello,we are trying to listen to can messages with our evaluation board. We are using a PCAN-USB adapter to play a can log to our eval board.When starting the PC program it says that there is no can buffer detected. We assume that somehow our CAN Tra...

0693W00000YAt9sQAD.png
LDini.1 by Associate II
  • 2132 Views
  • 3 replies
  • 1 kudos

Unable to TX on NUCLEO-ST32G491RE FDCAN1

I am trying to get CAN working on the STM32G491RE. I happily worked with CAN on STM32F4xxx micros, but the landscape seems to have changed on the STM32G491RE.The presented code is from a minimal project for the NUCLEO-STM32G491RE board. It is in defa...

JBend.6 by Associate III
  • 1249 Views
  • 0 replies
  • 0 kudos

SO8N STM32G031C6 USART not working.

I'm trying to setup an USART for a very small MCU of the STM32G0 family, the MCU it's theoretically being programmed, but the USART is not responding, I configured the MCU just like I did in other projects (of bigger MCUs), I'm not able to find what ...

0693W00000YAa9tQAD.png 0693W00000YAaAhQAL.png
fancyrat by Associate III
  • 8155 Views
  • 18 replies
  • 1 kudos

Resolved! STM32CubeMX 6.7.0 does not configure SDMMC DMA correctly

I am having an issue similar to https://community.st.com/s/question/0D53W000027iXpbSAE/spi-dma-configuration-generated-by-stm32cubemx-does-not-work but with the SDMMC peripheral rather than SPI.I have an STM32CubeMX project targeting the 32F746GDISCO...

FPlow.1 by Associate II
  • 2001 Views
  • 2 replies
  • 0 kudos