2022-06-01 6:10 PM
Hello, I'm programming using STM32H753. But I realized that the chip I chose when I was creating the project was STM32H743. Is there any way to change the chip settings in a project that has already been created? Should we re-create a new project unconditionally? Answer me. Thank you.
Solved! Go to Solution.
2022-06-02 1:28 AM
Hello @Ekim.1 ,
Thanks for your feedback,
There are two methods to change an MCU by CubeMX. For more details, please check my answer in this thread Changing from STM32F769NIHx to STM32F769BGTx.
PS: Unfortunately the List Pinout Compatible MCUs is bugged in v6.5.0 but it will be fixed. I would advice you to use the import method if you are working with v6.5.0.
I hope this helps !
If your issue is solved, please close this post by clicking the "Select as Best" button. This will help other members of the community find this response more quickly :)
Sara.
2022-06-01 11:20 PM
Hi @Ekim.1
I think there is no such kind of option to change the chip, if once the project is created .ioc file will be generated which is particular for that controller only.
If you think that this is best, select as best so that other's can find out easily.
2022-06-01 11:39 PM
Good news: there is a way in STM32CubeMX by pressing Alt+L or drop down the Pinout menu in the Pinout & Config tab.
Bad news: Some reported that the feature is sluggish or even broken in the current version, so you may try several times.
hth
KnarfB
2022-06-01 11:49 PM
Hi @Ekim.1 ,
Unfortunately, for the moment, the STM32CubeMX is not able to migrate a project to another STM32.
Best Regards
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-06-02 12:03 AM
You can create a new empty project and import a old one
2022-06-02 1:28 AM
Hello @Ekim.1 ,
Thanks for your feedback,
There are two methods to change an MCU by CubeMX. For more details, please check my answer in this thread Changing from STM32F769NIHx to STM32F769BGTx.
PS: Unfortunately the List Pinout Compatible MCUs is bugged in v6.5.0 but it will be fixed. I would advice you to use the import method if you are working with v6.5.0.
I hope this helps !
If your issue is solved, please close this post by clicking the "Select as Best" button. This will help other members of the community find this response more quickly :)
Sara.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.