2022-06-01 11:20 AM
The original param description:
* @param num FIFO number
* This parameter can be a value from 1 to 15
15 means Flush all Tx FIFOs
According to stm32h7 reference manual, it should be:
* @param num FIFO number
* This parameter can be a value from 1 to 15
16 means Flush all Tx FIFOs
:beaming_face_with_smiling_eyes:
2022-06-02 9:09 AM
Hello @oneshot.triplekill@qq.com ,
Thanks for your feedback,
This is not a CubeMX issue, the stm32h7xx_ll_usb.c file is copied and not generated by MX. I see your point, there is indeed a mismatch between the Reference manual and the usb driver file.
I am adding @Amel NASRI to the loop to further check this issue.
Sara.
2022-06-02 1:02 PM
ahaha, thanks .:beaming_face_with_smiling_eyes:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.