With this configuration :nbr of conversion : 2scan conversion mode : EnableContinious Conversion Mode : cannot set to Enable !!!Discontinious Conversion Mode : ucannot set to Disable !!!Unless I am mistaken, I see no indication in the STM32U5 referen...
With STM32CubeIde 1.9.0, open and change some settings in the IOC file, save your changes, and then click yes when a popup asks you to generate the code. At the end of the code generation, the IOC file is marked again as an unsaved file!
STM32CubeIDE Version: 1.9.0With the STM32CubeMX : Version: 6.5.0-RC4 and a project for STM32U585in the "project manager/advanced settings" tab, a line is missing to activate the "register callback" for the OCTOSPI interface best regards
Impossible to launch the debugger with the following configuration:STM32CubeIde1.7.0Target Nucleo-U575ZI-QST-link : Version: V3J8M3Build: Apr 9 2021 20:49:40See log filesSTm32cubeProg 2.8.1 can connect to the board successfully.What is wrong ?BUG ?
In file generated by CubeMx when creating a new project, the SystemInit function does not set the register of the interrupt vector table (SCB-> VTOR) !!! The default value is zero, which causes a crash on the first interrupt trigger, i.e. the code lo...
Hello Khouloud,Yes, this is the same problem.I ‘m working with STM32CudeIde 1.9.0 with a STM32Cube example project (STM32U585).1. Import example project2. Open IOC file, and change one settings3. Click save button (menu bar) -> (file s...
I confirm the behavior (bug),open and change some parameters in the IOC file, save your changes, regenerate the code, at this time the file is saved. At the end of the code generation, the IOC file is again marked as an unsaved file!And when you comp...