STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1564 Views
  • 0 replies
  • 2 kudos

DFDSM injection conversion triggered via internal timer.

Hello, I am trying to do an injection conversion of the DFSDM peripheral with the read process being triggered via an internal timer (TIM1) utilising the HAL drivers. Specifically, I want to set the counter to count up and trigger the read process ev...

SJohn.5 by Associate II
  • 3307 Views
  • 1 replies
  • 0 kudos

Resolved! Similar question to "I'm a STMCube Newbie. I'm under the impression when I set up the clocks in STM32CubeIDE, it should generate all the clock configurations. Right now I'm not getting the RCC_PeriphCLKInitTypeDef PeriphClkInit = {0}; Should it be there."

Does anyone have the same issue? Link to a similar question:https://community.st.com/s/question/0D53W0000260fFASAY/im-a-stmcube-newbie-im-under-the-impression-when-i-set-up-the-clocks-in-stm32cubeide-it-should-generate-all-the-clock-configurations-ri...

JChoi.12 by Associate II
  • 1732 Views
  • 3 replies
  • 0 kudos

Cube MX FreeRTOS Tasks vs Threads confusion

Cube MX seems to constantly confuse FreeRTOS Tasks and Threads.Term Tasks is being used where Threads are being actually configured.In FreeRTOS Tasks and Threads are two different beings.This is super confusing.

0693W00000aH9uzQAC.png
TDJ by Lead
  • 9574 Views
  • 8 replies
  • 0 kudos

STM32CubeMX, STM32F7 and CMSIS RTOS2 work flow?

I created project using ARM MDK (Keil) tool chain where I installed STM32 FW Pack and then using MX Cube to create main.c, stm32F7xx_it.h and stm32F7xx_it.c. I was not using any OS. Application is working ok. Now I am trying to add CMSIS - RTOS2 so I...

Importing a new .ioc in an existing project

We have a project that was working with a demo board with a different micro than our final project uses. We imported into CubeIDE an ioc generated by CubeMX by our hardware engineer. We did a bit of work on the project to include source from a vari...

AJone.5 by Associate III
  • 7770 Views
  • 8 replies
  • 0 kudos

STM32G030F6 BOOT0 and SWCLK shared

HelloI have a bunch of STM32G030F6 and they are in TSSOP20 package.I used SWD and BOOT0 pins to program L433 and want to do the same on G030F6However, unlike same TSSOP20 package F070F6 has, G030F6 share BOOT0 pin with SWCLK.19th pin of STM32G030F6 i...

0693W00000aIgShQAK.png
MKanc.1 by Associate III
  • 1596 Views
  • 1 replies
  • 0 kudos

Resolved! What is the significance of SRAM Bank swapping?

Hello all,While configuring the FMC SRAM configurations for STM32H747 MCU I found the option for bank swapping.As I see the reference manual I understand that the chip select configured interchanges it's address with that of the SDRAM bank addresses....

Aarra.1 by Senior
  • 4448 Views
  • 4 replies
  • 0 kudos