STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1601 Views
  • 0 replies
  • 2 kudos

Resolved! Updating LSE Drive Capability does appear to work

Hi, I recently had to update the LSE Drive Capability from "low drive" (0x00) to "medium high drive" (0x02) for an STM32U575 project. After making this change in STM32CubeMx and programming the micro with the newly generated code, I noticed the updat...

AGula.1 by Associate
  • 1539 Views
  • 1 replies
  • 0 kudos

STM32F103C8T6 + MAX30003

I'm using STM32F103C8T6 controller and I want to connect MAX30003 breakout board. Which preferences it's better to use for the best performance (STMCubeMX)? Can I communicate it with an SPI slave using the UART1 synchronous mode (configured with Cube...

MGGd.1 by Associate II
  • 1535 Views
  • 1 replies
  • 0 kudos

CMSIS with Keil

Hi, I have created a project with Keil compiler (v5.17 )and I'd like to use the CMSIS driver for SPI.When I selected CMSIS in RTE, it tells me that I need CubeMX for configuring the HAL.I used CubeMX for generating the code, but there are many errors...

LBern.5 by Associate II
  • 5240 Views
  • 5 replies
  • 0 kudos

CubeMXIDE multiple definition bug still here

FreeRTOS project: code generated includes code in Drivers/CMSIS/Device/ST/STM32F4x/Source/templatesFile is of definitions, likely stm32F4xx.hThis conflicts with the file included at Drivers/CMSIS/Device/ST/STM32F4x/Include.This seems to only happen ...

Anybody else seen when in CubeMX selecting Enable SD register Callbacks also causes SDRAM register callbacks to automatically flip to enable when saving and generating code?

STM32CubeIDEVersion: 1.12.0STM32CubeMX: Version: 6.8.0-RC4I think this is a BUG!When in CubeMX perspective in CubeIDE, in the project manager Advanced tab, in the Register Callback window, if you ENABLE the register callback for SD and save or gener...