STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1564 Views
  • 0 replies
  • 2 kudos

Resolved! CubeMX 6.5 bugs

Hi,I would like to report 2 bugs.I created a blank new project for STM32G030F6P6. When I try to enable USART1, it says "Unknown conflict". See the attached screenshot.For STM32L452RET6, when I set LSE drive level other than the default with LL driver...

0693W00000Np6GdQAJ.png
a.gajdacs by Associate II
  • 2824 Views
  • 6 replies
  • 0 kudos

Input pin stm32g0 always remains low

I am learning the stm32 using a stm32g070cbt6 micro controller with custom PCB with keil. When I add an external pull-up to the pa4 pin and use it as an input pin. Nevertheless, when I read the pin, the output is low always, even though on the hardwa...

Ali110 by Associate II
  • 4210 Views
  • 4 replies
  • 0 kudos

Resolved! Problem when generating code in STM32CubeMX

MCU: NUCLEO-L433RC-PSTM32CubeMX version: 6.8.0MDK-ARM Community version: 5.38.0.0Java version: 8 update 361 (build 1.8.0_361-b09)When I try to generate code I get this message:The Code is successfully generated under : C:/Users/.../project Project la...

MS.23 by Associate II
  • 4786 Views
  • 2 replies
  • 0 kudos

Resolved! NUCLEO-L4P5ZG USB device VCOM hangs after updating from STM32CubeIDE v1.9.0 to v1.10.0. The problem still exits in v1.11.2.

I have a program running on NUCLEO-L4P5ZG board. The USB device VCOM runs fine on STM32CubeMX v6.5.0 (STM32CubeIDE v1.9.0). It was broken since STM32CubeMX v6.6.0 (IDE v1.10.0). The problem still exists in STM32CubeMX v6.7.0 (IDE v1.11.2). My workaro...

CZhan.8 by Associate
  • 2325 Views
  • 1 replies
  • 0 kudos

What happens to FreeRTOS code generation?

Today my STM32CubeIDE does an update to the Version: 1.11.0 (Build: 13638_20221122_1308 (UTC) ) including the CubeMX Version: 6.7.0-RC2 (Build: 20221118-1646 (UTC))Using the FreeRTOS Middleware the generation of the main file has a big bug. There wil...

TManiac by Associate III
  • 5794 Views
  • 8 replies
  • 1 kudos

Resolved! Bug in CubeMX generating Makefile, missing some CPU info.

I did not tested if this is specific to all MCU but for U5 familly this is sure:How to reproduce : Launch cubeMX, (6.7.0)select U5 board like nucleoGo to project manager, and select under Toolchain - Makefile.--> Bug, the Makefile genereted is missin...

Bertha by Associate III
  • 2318 Views
  • 2 replies
  • 0 kudos