User Activity

I have a custom board with STM32G070RB micro. I programmed the board several times for debugging in the development phase using theST-LINK//V2 in CubeIDE.Now I would like to generate a .bat file to program the boards, but I am facing some problems.My...
I am using STM32G070RBTX micro configured for ADC with DMA. My project works well configured with CubeIDE version 1.8.0. However after I updated to 1.9.0, the ADC Continuous Conversion Mode cannot be Enabled from CubeMX. It force to use Discontinuous...
Posted on June 06, 2017 at 09:51Hi!I am using the SPWF04S module configured in MiniAP mode. I've created a file in RAM memory using the AT+S.FSC command.I am reading the file using the AT+S.FSP command. After about 450-500 successfully readings, the...
Posted on May 17, 2017 at 14:28I am trying to send data from the browser to the module using POST request with output_demo.html. The POST request is limited to 64 bytes, so I cannot send more than 64 bytes with a POST...If I send 65 bytes, the last ...
Posted on May 11, 2017 at 15:04Hi!I am using the SPWF04SA module. I am trying to create dynamic pages. My webpage is done and it works. I'm having problems with updating the tokens buffer using the AT+S.INPUTSSI command as described in the AN4965 Ap...
Kudos from
Kudos given to