STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1628 Views
  • 0 replies
  • 2 kudos

Resolved! Linked Resources update issue using STM32CubeIDE

Hello,I'm currently working with the STM32H745I-DISCO board, using STM32CubeIDE and STM32CubeMX v1.14.0 for peripheral initialization. Initially, I enabled SDMMC1 on the Cortex-M7 core, which worked well - the necessary resources were added to my pro...

Question about ADC versus GPIO Analog

Posted on April 03, 2015 at 04:23In STM32CubeMX, when I click on a pin, the following are two of the choices amongst others are presented to me. I want to understand what the difference is between ADC1_IN0 versus GPIO_Analog. I have looked through n...

Resolved! CubeMX SPI data size bug?

In CubeMX when configuring a SPI peripheral I can only choose either 8 or 16 bit, but the STM32G491 reference manual says data size can be from 4 to 16 bit. Is this a bug in CubeMX?(using the newest CubeMX version)

decalvus by Associate II
  • 2805 Views
  • 4 replies
  • 0 kudos

STM32CubeMX Won't start after Windows update - Dec 2023

I went to use STM32CubeMX and I get the splash screen then nothing. I downloaded and installed the latest version V6.10.0 and still the same. I am running windows 10 professional. Does anyone else have this problem ? I wonder if there has been a Java...

patm by Associate II
  • 6688 Views
  • 7 replies
  • 0 kudos

CubeMX placing MX_LWIP_Init() in first listed RTOS task.

Hi everyone. Maybe this my doing or an oversight by ST?CubeMX places the MX_LWIP_Init(); function in the first listed RTOS task witch is far from ideal. In my case the "first task" is dynamically created depending on a multitude of different factors....

XD by Associate III
  • 1891 Views
  • 2 replies
  • 2 kudos

Default value for targets in CUBEMX

Hello everyone,I'm currently involved in a project and I'm aiming to analyze the peripheral initialization parameters of a specific target by examining the .ioc file. I parsing through the ioc file like a text file. While the .ioc file contains detai...

ADani by Associate III
  • 1957 Views
  • 3 replies
  • 0 kudos

CubeMx Interface Bug

Hi,I am facing an issue with the cubeMx UI. After using it for some time about 10 to 15 minutes, the UI is overlapping each other. Then I need to close the UI and start again. Again the issue is present after some time. CubeMx Version : 6.10.0 

albinv06 by Associate
  • 2701 Views
  • 1 replies
  • 1 kudos