STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1584 Views
  • 0 replies
  • 2 kudos

STM32H743ZI ETHERNET+USB USING

 I am USING BOTH ETHERNET+USB IN STM32H743ZI  WHEN I CONNECT ETHERNET THEN NORMAL BUFFER UPDATE PROBLEM OCCURING  cnt_10=11;                                                      ///this buffer is updated     MX_LWIP_Init(); //ETHERNETHAL_Delay(10);cn...

SITARAM by Associate III
  • 1800 Views
  • 2 replies
  • 0 kudos

STM32CubeMX Configure USB Host

Hi I am currently using STM32CubeMX version 6.4.0 to configure the STM32H7 series. I have configured it as a USB host, and I want to send messages through USB. Therefore, I called the USBH_CDC_Transmit function. However, when this function reaches th...

lekaho by Associate
  • 1763 Views
  • 2 replies
  • 0 kudos

Meaning of IP in STM32CubeMX

Posted on June 20, 2015 at 04:17What is the meaning of IP in the STM32CubeMX software? I looked at the documentation, but I don�t find it and google obviously show me TCP/IP. Thank you. #cube #stm32cubemx

vinicio by Associate II
  • 4823 Views
  • 7 replies
  • 0 kudos

Resolved! Pin conditions during ST bootloader selection

Hello everybody,for first time flash programming of private CAN bootloader i want to use the ST bootloader.Despite of the nBoot_SEL Bit i can flash data if the flash is empty.The bootloader mechanism is shown in Figure 55 in the AN2606.Now the questi...

Kai4 by Associate II
  • 1823 Views
  • 2 replies
  • 0 kudos

Resolved! Effect of CubeMX DEBUG Settings

Other than reserving pins for the hardware-implemented debug interface (Fig. 1), what are the effects of the highlighted settings of the "Trace and Debug" category of CubeMX (Fig. 2)? Fig 1: Debug infrastructure (RM0433) Fig 2: CubeMX Trace and Debug...

dmocom_2-1709880966211.png dmocom_1-1709880891568.png
dmocom by Associate II
  • 2856 Views
  • 3 replies
  • 3 kudos

Resolved! How to enable LWIP_SOCKET on Nucleo-F767ZI board in CubeIDE

Hi,I have a Nucleo-F767ZI board, and am trying to configure it to use its LEDs, USART3 which is the virtual com port of the ST-Link on the board, and eth, I added LWIP, but I am unable to enable the LWIP_SOCKET as it requres to enable LWIP_NETCONN, b...

Chao_1-1709634060539.png
Chao by Senior II
  • 2595 Views
  • 3 replies
  • 0 kudos