Hello, what is meaning of the "Modified" column in GPIO configuration? When given pin is considered as modified? I am not able to find that information in CubeMX user manual...
Is this possible to use internal USB OTG HS PHY in FS mode in STM32F429NI with 1.8V VDD? Internal USB OTG FS PHY needs VDD>2.7V. USB OTG HS in HS mode needs external PHY connected via ULPI. Would OTG HS PHY in FS mode work with VDD = 1.8V?
Hello Sara,Thank you for your reply.I am afraid it is not such simple... These flags are active even when I open the .ioc file of the project where the configuration code was previously generated with default settings for Nucleo F411, project was com...
Hi, one more thing in this topic - I have found such information in datasheet (pictures below).It looks that USB OTG HS (controller only; not FS transceivers) should work with VDD=1.8V. So it should be possible to use USB HS only (with external trans...
Hi Khouloud,Thank you very much for fast and detailed answer!Yes, my question was about using integrated transceiver for FS operations from USB 2.0 FS/HS device/host/OTG controller. I would like to use this integrated transeciver for communication wi...