STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1628 Views
  • 0 replies
  • 2 kudos

OPAMP on STM32G431KB

Hi, Master:Hello, I want to use the opamp amplifier function of the g431kb board to connect an external gain circuit and use standlone mode. Can I use it after downloading my MXsoftware generate code?I set the OPAMP1_P (PA7) input to 2.5V (DC power s...

scope_12.png

Fixing code generation in CubeMX: Tickless functions

Hello, when using CubeMX + STM32WB + BLE, I noticed that if the BLE feature is enabled in CubeMX, a file called freertos_port.c is created in the project. This file includes the functions void vPortSuppressTicksAndSleep(TickType_t xExpectedIdleTime) ...

JJRR by Senior
  • 2614 Views
  • 4 replies
  • 0 kudos

STM32F4 CAN Bus example using HAL Library

Posted on April 22, 2016 at 18:51Hello,   i am new to HAL Libraries. i am learning to work with CAN BUS using HAL Libraries. Can any one please post an example of STM32F CAN BUS using HAL Libraries.as it will help to have an idea how should we progr...

ninad911 by Associate III
  • 35699 Views
  • 18 replies
  • 0 kudos

Resolved! IOC file lifetime in project development

Hi, how long do you recommend that we keep our development project's in-sync with the IOC file used to generate them? Setup:MyNewDemo.ioc is used to create a demo monitoring the UART that responds to to toggle requests for its GPIO Scenario #1:Periph...

jreina by Associate III
  • 2585 Views
  • 3 replies
  • 2 kudos

STM32F407 ETH Problem

Hi Everyone,I cannot choose the speed of the Eth. Pls see the pisture below. The version of the STM32CUBEMX that I downloaded is the latest.Best regards,Jason Pls see the picture.Best regards,Jason

STM32F407VET6 ETH.png
Xinda by Associate
  • 1014 Views
  • 1 replies
  • 0 kudos