User Activity

 Hi all,currently I am Working with STM32H743BIT6 & TouchGFX  I am facing issue with screen flickering,I am using OpenH7XXI-C board with 7inch capacitive LCD(F) display (Working Fine No issue )But With  10.1inch capacitive LCD(D) display (NOT Working...
 I am using CUBEMX Version   6.10 STMCUBE IDE                        1.16.0FW version                               F7V1.17.0Enabled LWIP ETH With FREERTOS CMSIS2same settings did with cmsis version 1 it's working but with cmsis version2 NOT WorkingI...
I Enabled LWIP DEBUG options in CUBEMXin lwipopt.h  /* USER CODE BEGIN 1 */ #define LWIP_DEBUG 1 /* USER CODE END 1 */ in main.c  int __io_putchar(int ch) { ITM_SendChar(ch); return ch; }  But I am not getting anything in SWVITM Data Console
Hi Team,I am Using STM32F7 nucleo board, I created project using ST CUBEIDE version 1.16.0.Note: NOT USING CUBEMX and RTOSI have taken a ref code for low level eth functions ethernetif.c and lwip.c.I Enabled Enable DHCP, Http and SSI it is working fi...
Hi Team,I am using STM32F7 nucleo board, CUBEMX version 6.10, FREERTOS CMSIS V2, LAN8742 Eth driver. I am working with LWIP stack  FULLDUPLEX 100Mbps configuration.configured MCU as a server and re-establish communication in LWIP default thread.1. ca...
Kudos from
Kudos given to