STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1559 Views
  • 0 replies
  • 2 kudos

Cube32 feature request, need to handle CPP files.

The support of CPP architectures in Cube32 is limited. While it would be nice if Cube32MX actually had CPP libraries, that's a long step.It's very possible, however, to integrate a C++ layer on top of the existing code, where C++ routines call C rou...

STM32CubeMX 6.11.1 released

STM32CubeMX 6.11.1 was released on st.com as well as an in-tool update patch. Main issues fixed in this patch: Ticket 176645 : STM32CubeMX V6.11.0 has lost the "JTAG (5 pins)" debug mode for all the STM32H7 series but the STM32H7Rx/7Sx microcontrolle...

Stm32H7 Ethernet issue

hello, Dose anybody have solution why Ethernet shut down randomly every few days? i'm working on ethernet (UDP/IP) without RTOS in keil, stm32cubeMX some old versions 5.4.0 FW versions 1.5.0 work fine but if i send data continuously for 5-6 days then...

PSONI.11 by Associate II
  • 3149 Views
  • 7 replies
  • 1 kudos

OLED SSD1322 DISPLAY

Hi there,I'm trying to use an NHD-2.7-12864WDW3 model OLED LCD that has SSD1322 driver. Im using m68 parallel interface.The MPU im using is Nucleo-F072RB and im using CUBEMX for adjusting it's settings and using KEIL IDE for coding. Whatever i done i...

0693W00000aIU3KQAW.png
Kannic by Associate II
  • 6741 Views
  • 7 replies
  • 0 kudos