STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1258 Views
  • 0 replies
  • 2 kudos

Resolved! CubeMX generates wrong configuration for STM32L071

  Hi everyone,I think STM32CubeMX is generating an incorrect configuration for STM32L071.In CubeMX → System Core → SYS → System power supply,I selected Power Regulator = SMPS (instead of LDO) and generated the project.After code generation, I get bui...

image.png image.png image.png
isikli by Associate III
  • 228 Views
  • 1 replies
  • 1 kudos

Resolved! I cannot enable DCMIPP interface pins

Hi,I am implementing DCMIPP configuration in that I am enabling the CSI but when I trying to enable the pin I cannot enable the the camera pins those pins are showing red. And I am unable locate .ioc file  for DCMIPP interface is there any .ioc file ...

Resolved! Missing files in generated code for USB Audio

Question for STM.Could you please advise what to do to make the environment generate audio files?Could anyone of you show me how to generate these files?They are generated for all classes except audio.I guess there should be these too.Alternatively, ...

image.png
konsul41 by Associate II
  • 1363 Views
  • 2 replies
  • 0 kudos

CubeMX SD card initialization bug

In the update to CubeMX version 6.17, the SD card initialization (in my case, SDMMC2) was changed, and the software goes into "Error_Handler()". In my project I use STM32H7B0VBT6, FATFS, not RTOS.Specifically, version 6.17:static void MX_SDMMC2_SD_In...

cb.7 by Associate III
  • 298 Views
  • 6 replies
  • 0 kudos

CubeMX Bugs

Version 6.16.1I have identified a number of bugs - collecting them here.  Note that these are time wasters, but there are workarounds - so they are not critical but would definitely aid in the usability/productivity of users.-If you use the XCube.AI ...

Resolved! STM32WL5MOC Wrong LSE Drive Config in Example

I used CubeMX to generate the "LoRaWAN_AT_Slave" example for the B-WL5M-SUBG1 board.I had some issues with it waking up from sleep and upon a few hours of debugging i found that the LSE Driver Config was set to LOW in the example application, but the...

SKäli.1 by Associate
  • 188 Views
  • 2 replies
  • 1 kudos