STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1564 Views
  • 0 replies
  • 2 kudos

Resolved! Please rescue cubemx!!!

The login function greatly affects efficiency!!!cubemx Version 6.11.1I just want to install the G0 pack. But I cann't login even using VPN.  My net works very well! So I can only download it from the official website and then install it locally.The S...

企业微信截图_17156801062692.png 企业微信截图_17156800895962.png 企业微信截图_1715682184593.png 企业微信截图_17156801248942.png
gtop.1 by Associate III
  • 3011 Views
  • 4 replies
  • 3 kudos

Resolved! CubeMX 6.11.1 Generation Code problem

Hello everyone.First, sorry for my english. I'm still learning, and i'm trying to write this text without using google translator.I found one problem in the Cube MX (already solved), in the generation code in a specific case, and I don't know where i...

CubeMXproblem.PNG

Resolved! Embedded ST-Link in NUCLEO Board

Hello,I have NUCLEO-H755ZI-Q ST Board. To initialize the board, I used the STM32CubeMX initialization code generator ("Start My project from ST Board").The Debug in this initialization is set to "Disable" (i.e., no Serial Wire or JTAG is active).How ...

Chaim by Associate
  • 1251 Views
  • 1 replies
  • 1 kudos

STM32PacketCreator Bug

When press enter after text on "Packet Description", Packet generated successfuly and did i uploaded to git. but it did not appierd on cube mx. after delete the enter from end of "Packet Description", it worked. 

nimaltd_0-1719638590282.png
nimaltd by Senior
  • 761 Views
  • 0 replies
  • 0 kudos

Running STM32CubeMX without GUI

Hi All,I am trying to setup a build pipeline for the STM32 platform to be able to compile projects in an automated fashion. So far, I have an .ioc file which I use the to generate the project using the STM32CubeMX commands which are invoked via the s...

ANath1_0-1717562433830.png
ANath.1 by Associate III
  • 8559 Views
  • 15 replies
  • 5 kudos

Resolved! I am getting this error message:   - Main Config: These peripherals still have some not configured or wrong parameter values:[FATFS,Verify...

Hi,While configuring STM32F446RE on CubeIDE for writing and reading on SD Card using SDIO mode (1 bit mode), when I'm generating code I get this error message :   - Main Config: These peripherals still have some not configured or wrong parameter valu...

meco54 by Associate
  • 2679 Views
  • 1 replies
  • 1 kudos