Skip to main content
Semer CHERNI
ST Employee
September 19, 2023
Question

STM32CubeMX 6.9.2 released

  • September 19, 2023
  • 0 replies
  • 3480 views

STM32CubeMX 6.9.2 was released on st.com as well as an in-tool update patch.

Main issues fixed in this patch:

  • Ticket 158577 - [Bootpath Config] env.bat add quotes to variable stm32tpccli
  • Ticket 158868 - [Bootpath Config] secure manager post build cmd must also generate a .bin file
  • Ticket 158979 - Wrong location of RAM in linker file for secure manager
  • Ticket 158982 - Secure Manager : missing secure manager api files in STM32CubeIDE generation
  • Ticket 159213 - Secure Manager : When enabling RTC MX does not generate SystemClock_config anymore
  • Ticket 159423 - [Boot path Config] Exception occurs when changing Boot Path reference location
  • Ticket 159633 - [Secure Manager] remove TPC access when "Secure Manager" Boot Path has been selected
  • Ticket 160247 - Secure Manager MX code generation on MAC produce wrong postbuild.sh

Where do I obtain STM32CubeMX 6.9.2 ?

This topic has been closed for replies.