STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1547 Views
  • 0 replies
  • 2 kudos

Resolved! Newbie with newbie problems Oscillator start up ?

Hi People, for the since start of year i've been setting up boards with Texas C2000 , and for the past 6 months infineon tri-core processors.  I may be changing jobs and it involves STM32 so i'm getting a head start. I have a STM32373C-EVAL , as i ne...

John_S_0-1726412883613.png
John_S by Associate II
  • 8218 Views
  • 16 replies
  • 4 kudos

Resolved! DSIHOST disabled in CubeMX for STM32F469...?

[SOLVED - I found the solution after posting]Hi,the STM32F469 has DSI but when I try to enable it in CubeMX it shows in Italic and greyed out and if I click on it cannot be enabled. See screenshots below.Why is that?How do I enable it?Thank you  

Ricko_1-1729917685233.png Ricko_0-1729917542498.png
Ricko by Senior III
  • 1124 Views
  • 1 replies
  • 0 kudos

CubeMX fails to generate project on apple Silicon

Hello, The project generation for CubeIDE fails on apple Silicon due to x86 compiled libraries org.eclipse.equinox.launcher.cocoa.macosx.x86_64_1.2.800.v20231003-1442/eclipse_11802.so' (code signature in 66ADAB06-1B30-301C-8ECA-7EDC8C31724D '/Applica...

Cordic Two Config

Hi,How can I set up two Cordic Configuration, because I want to calulate using two different function. CORDIC_ConfigTypeDef sConfigSine;CORDIC_ConfigTypeDef sConfigPhase;CORDIC_ConfigTypeDef sConfigCosine; I tried to set up 3 different cordic configu...

James613 by Associate II
  • 917 Views
  • 0 replies
  • 0 kudos

USBX standalone on STM32H5

I'm trying to use STM32CubeMX to generate a USBX Device CDC ACM in standalone mode (without using ThreadX).I'm using a Nucleo-H563ZI to test with. I can do this with ThreadX and get it working, but when I try the standalone configuration it doesn't w...

iguffick2 by Associate III
  • 6303 Views
  • 5 replies
  • 1 kudos

Undefined reference to 'HAL_RTC_Init' problem

Hi, I want to use the RTC. ( Use STM32F429ZI Discovery board )​So, I set 1. RCC-> High Speed Clock Cystal/Ceramic Resonator RCC-> Low Speed Clock Cystal/Ceramic Resonator2. Clock Configuration -> RTC Clock Mux -> LSE3. Pinout & Configuration -> Ti...

0693W00000JMfiJQAT.png 0693W00000JMfjbQAD.png 0693W00000JMfiLQAT.png 0693W00000JMflrQAD.png
지한.1 by Associate II
  • 7557 Views
  • 5 replies
  • 0 kudos