STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1547 Views
  • 0 replies
  • 2 kudos

Resolved! SPI2 Frequency of the STM32F469BIT7

EMB1428QSQ/NOPB is used which has the frequency of the 1.1MHz fclk and the SPI2 of STM32F469BIT7 is going as a clock to it. I need the minimum value of the SPI2 master that can be fed to the EMB1428QSQ/NOPB. Also, where can I find the minimum frequen...

Cannot install middleware

Hi  I am using STM32 CubeMX and am trying to add the LoRaWAN package but have this message ( see below). I am not sure how to fix ?Any one have any guidence on this? 

Screenshot 2024-10-31 at 21.43.07.png
fabltd by Associate III
  • 1041 Views
  • 1 replies
  • 0 kudos

MQTT over MbedTLS for AWS

Hi!My goal is connection of STM32 mcu to Amazone web service.I was wonderful bu Cube and generate a first application (freertos with lwip) for nucleo-f767zi board. There are function like mqtt_client_connect and mqtt_publish in code that was generate...

SZhuk.1 by Associate II
  • 5717 Views
  • 6 replies
  • 0 kudos

Resolved! CubeMX LWIP ethernet_link_thread bug

I am using stm32f407zg board with DP83848 ethernet PHY chip. CubeMX generates code with LWIP for FreeRTOS. App used to answer ping successfully when it starts with connected eth cable only and stops after its reconnecting. After some investigation i ...

el_d by Associate II
  • 12371 Views
  • 12 replies
  • 4 kudos

Problems creating a relocatable git project

I am desperately trying to seed a production project involving multiple engineers (and across multiple companies) and am having great difficulty getting the project to build once it has been pushed to a git repository.  The difficulty involves the cr...

zcab911 by Associate
  • 933 Views
  • 1 replies
  • 0 kudos