User Activity

Hi,In the project that I saved-as (to rename) the DEBUG was set to JTAG (5 pins).After updating to STM32CubeMX version 6.11.0 I observe the JTAG (5 pin) option is unavailable.Below change (i.e. switched DEBUG to JTAG (4 pins))  was made by software a...
Hi @Imen.D  , @Khouloud ZEMMELI ,After updating the STM32CubeIDE to version 1.15.0 (today) I am observing below warning.The LD file has not changed. It has RAM and MRAM RWXC:/ST/STM32CubeIDE_1.15.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.extern...
Dear @Khouloud ZEMMELI , @Imen.D  ,Please connect me with someone to help resolve the below concern.I have enabled all possible warnings in STM32CubeIDE.I however just want to disable warning for one large sized constant array (possibly using #pragma...
Dear @Khouloud ZEMMELI , @Imen.D , @Pavel A. ,Please connect me to someone who can help resolve issue with format specifiers mentioned in inttypes.hI am building code for STM32H7xx microcontroller. Concern 1:Is it possible to update inttypes.h, as I ...
@Khouloud ZEMMELI, @Imen.D ,I am aware that FMC MRAM/SRAM (connected to NE1) (or even others) cannot be used until the main clock is configured, Pins clocks are configured, and FMC registers are set.Please help me connect to someone who can help me u...