STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1547 Views
  • 0 replies
  • 2 kudos

Failure problem during development of LSM6DSR output Euler angles

使用cubemx选用LSM6DSR的SPI通信、选用motion_di库,选用倾斜解算应用导出的项目文件(在连接文档中有压缩包)。导出后我删除了一些我不需要的操作以及一些必要部位的标志位,能正常产生数据但我无法确定数据是否正确,并且在两次或者两次以上循环后会跳入硬故障程序。具体如文档,wo'xiang'温'yi'xiaTranslation to English: Using cubemx with the LSM6DSR SPI communication option, the motion...

USART in synchronous mode

So I have a busy board, and SPI MISO is occupied.I would like to communicate in synchronous fashion with an FPGA.Can I Make this USART peripheral work in a SPI Master full dulex, synchronous mode?The baud rate seems to be limited in CubeMx, is this b...

_SDIO_GET_FLAG Error

So I'm using a SDIO connection to write some files to the SD card (MCU STM32F446Vet6).Using the PC8-PC12 lines. Using the FATFS and SDIO from CubeMX. In main.c file have this sniped of code /* USER CODE BEGIN 2 */ if(f_mount(&SDFatFS, (TCHAR const*...

MBolo.1 by Associate III
  • 1542 Views
  • 1 replies
  • 1 kudos

Unable to compile FreeRTOS project

Hello,I am currently experiencing issues with compiling a Makefile project for the STM32F103C8T6, generated by STM32CubeMX. The project has the FreeRTOS middleware enabled, with CMSIS V2.Compilation of the generated code results in these errors:https...

j0of by Associate II
  • 5867 Views
  • 7 replies
  • 1 kudos