STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ChibiOS/RT demo application for the STM32VL-Discovery

Posted on November 27, 2010 at 15:24Hello, In the latest ChibiOS/RT release 2.1.4 I added a specific demo application for the STM32VL-Discovery board. The demo application introduces to the use of the RTOS kernel and of the HAL, PAL, PWM, ADC, SPI a...

Download and Erase don't work in Keil

Posted on September 26, 2010 at 20:13In Keil, if I go to Flash->Download, it says ''loaded ... DISCOVER.axf'', the red COM LED blinks couple of times, and then stays red. The whole thing seems to be hanging. When I power-cycle the device, the old fi...

USART problem

Posted on November 16, 2010 at 21:41Hi, I've managed to get the example program working which transfers a buffer of text from usart2 to usart3. When I try and output on usart2 to a PC however it seems as if the baud rate is wrong. I just get garbage...

求助stm32f105vc çš„otg usb host,å�‘é€�一个setup包时示波器有波形输出,但是通é�“会自动å�œæ­¢å¹¶äº§ç�?Ÿä¸­æ–­ã€‚这是正常的å�—?

Posted on November 17, 2010 at 09:26求助stm32f105vc çš„otg usb host,å�‘é€�一个setup包时示波器有波形输出,但是通é�“会自动å�œæ­¢å¹¶äº§ç�?Ÿä¸­æ–­ã€‚这是正常的å�—?

ADC Not Working

Posted on November 11, 2010 at 11:14The original post was too long to process during our migration. Please click on the attachment to read the original post.

ezrab by Associate II
  • 1453 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.