STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to Enable BusFault, MemManage Interrupts

Posted on June 20, 2011 at 12:31Hi, Is it neccessary to do something to enable BusFault and MemManage Interrupts, or are these active as per default? I.e. the HardFault interrupt is always enabled, the only thing I need to do is add a HardFault_Han...

Pin mapping USB and JTAG/TRACE

Posted on June 17, 2011 at 02:02Hi everyone,I've just ordered the STM3220G-EVAL, but while waiting for it to arrive, I'm looking at pin mapping for my application.In particular I have a couple of questions in regard to USB FS, and JTAG/TRACE.USB FS=...

use_no_semihosting_swi doesn't work

Posted on June 17, 2011 at 19:25I am running the simplest sample program that came with the Standard Peripheral Library Template (that lights 4 LEDs, displays a line on the UART, and 3 lines on the LCD).  Using the Keil tool chain, I turned off Use ...

mschwab by Associate II
  • 3206 Views
  • 2 replies
  • 0 kudos

uIP Stack for STM32F107

Posted on June 17, 2011 at 14:49Hello everybody,Do you have any idea where to find an code example of using uIP stack for UDP communication?. Basically, what I want to do is establish a two way communication between my PC and the stm32, based on UDP...

Why STmicro not fixes errata in new revisions ?

Posted on June 13, 2011 at 18:01One really sad and annoying issue regarding otherwise very good ST MCUs, are ST behaviour/policy of not fixing errata in new chip revisions, inheritance of IP/peripheral blocks including erratic functions and NOT fixi...

weird by Associate II
  • 1343 Views
  • 2 replies
  • 0 kudos

The question on the stm3210b_eval_lcd.c

Posted on June 14, 2011 at 03:30In stm3210b_eval_lcd.c Why use static __IO in this definition TextColor and LCDType ? Put another wayI understand the static definition of the prefix stands for a static variable?but static sFONT and static __IO shoul...

lxnisme by Associate II
  • 2996 Views
  • 7 replies
  • 0 kudos

stm32 and android

Posted on June 13, 2011 at 07:58Hi all, does it exist libraries and a toolkit for STM32 able to connect through Bluetooth smart phones android based to STM32? Is there any plan to devolop it?brazov2

brazov22 by Associate II
  • 1968 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.