STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Interrupts don't trigger on new board with same code

Posted on August 08, 2011 at 17:33Our STM32 chip isn't taking interrupts after a normal power reset, or a pin reset... but it will when it's in debug mode, or when (accidentally) Vdd was shorted after startup.We recently respun the board with our AR...

kuhnzaga by Associate II
  • 3579 Views
  • 9 replies
  • 0 kudos

STM32 , DMA Transfer Complete Interrupt never triggers

Posted on August 28, 2011 at 22:37 Hello guys, I spent all the afternoon trying to just trigger an interrupt. The example is easy, I have FreeRTOS 7.0.1 running with a periodic task which writes a sequence towards USART2 employing the DMA1 (chan...

noeth3r by Associate
  • 1219 Views
  • 1 replies
  • 0 kudos

Loss of synchro while transmitting data using STM32

Posted on August 27, 2011 at 10:53Dear STM32 users, I am facing an issue not related to the micro, it seems to be a general topic when transmitting data over usart. In my application I have an STM32 micro that will transmitt and receive data to/from...

po by Associate II
  • 1310 Views
  • 3 replies
  • 0 kudos

ADC value in buffer

Posted on August 25, 2011 at 16:49Hello, I have a buffer char buf[128]; And when I use ADC it gave me values like 1204 for eg. by ADC1ConvertedValue[1] which is the channel 1 for me. How could I store the 4 characters 1,2,0 and 4 into my buffer? I h...

cyril2399 by Associate II
  • 1889 Views
  • 3 replies
  • 0 kudos

Eclipse IDE+Code Sourcery+OpenOCD+ST-Link/V2?

Posted on August 25, 2011 at 13:58Dear All, We are using STM32F107RC microcontroller for our product having an ethernet interface. We are using Eclipse IDE with OpenOCD. Will I be able to use ST-Link or ST-Link/V2 with these utilities for programm...

rajmathi by Associate
  • 1006 Views
  • 2 replies
  • 0 kudos

Problem with Input Capture in STM32F103RBT6

Posted on August 22, 2011 at 15:25Hi all! I'm using STM32F103RBT6, board Olimex STM32-H103 and i'm trying to create an IR receiving firmware. I'm using Input Capture mode TIM1-Channel1 with the specs below: /*/*/*/*/*/*/*/*/*/*/*/*/*/*/     TIM_ICIn...