STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SOLVED. USBH_BulkReceiveData problem

Posted on January 31, 2012 at 13:25The problem is found, but there there is an eternal interrupt loop when NAK from device, so there is an another patch is required for the host lib, 'cause there is no wayto know when the device finished data transf...

0690X00000604xqQAA.png
dzuikov by Associate II
  • 1185 Views
  • 1 replies
  • 0 kudos

1MHz timebase messing with PWM frequency

Posted on January 30, 2012 at 08:06(I'm posting this ''again'' as it doesn't look like it posted. :-/)Hi,I've been using the PWM Output example for my PWM jobs. The timebase was setup as follows (with variables replaced with actual perimeters):  Pre...

Timer (TIM2) goes twice as fast as expected

Posted on February 03, 2012 at 21:38I can't tell if this is a ''feature'' or some strange incongruence.  I am using an STM32F103ZG (on STM3210E-EVAL board).  - The clock is set to 48 MHz, as USB is being used.  - The APB1 bus is set to 12 MHz (divid...

jpnorair2 by Associate II
  • 2720 Views
  • 4 replies
  • 0 kudos

ucLinux in STM32F407 (on STM3240G-EVAL)

Posted on January 26, 2012 at 07:03How can I run ucLinux on STM32F407 (STM3240G-EVAL)???In an3012 there are bootloader (hex) and kernel ucLinux (bin/dfu), but its for stm32f101/f103. 1) Where can I get it for STM32F407 ? How can I make bootloader to...

0690X00000604xgQAA.png
akk_inet by Associate II
  • 2798 Views
  • 5 replies
  • 0 kudos

uLinux for STM32F2/4

Posted on February 02, 2012 at 08:21Hello all. There is a problem to run uLinux for STM32F2/4. The run of uLinux is possable by the spesial boot loader. This boot loader works only for STM32F1xx controllers. It is in the web. So, where can I get the...

yagov by Associate II
  • 1233 Views
  • 2 replies
  • 0 kudos

Stepper motor

Posted on July 20, 2009 at 09:22Stepper motor #stepper-motor #stepper-motor-driver

finnb by Associate II
  • 2815 Views
  • 6 replies
  • 0 kudos

how to use timer _ interrupt

Posted on January 26, 2012 at 17:58i am beginner about programming on  stm32l discovery board.  this is my first time  programming on stm microcontrollers.  I can open led. close led.  i can use lcd on it. but i want to  do that.i have   int i=0;   ...

accounts by Associate II
  • 3684 Views
  • 8 replies
  • 0 kudos

SPI TXE flag interrupt

Posted on January 31, 2012 at 06:01I'm using the SPI TXE interrupt.  My ISR simply checks to see if there is anything more to transmit in the buffer.  If there is, it sends it, moves the buffer pointer, and returns.  If there isn't anything left to ...

shannon2 by Associate II
  • 3215 Views
  • 4 replies
  • 0 kudos

STM32F4Discovery / RS232 CABLE

Posted on January 29, 2012 at 22:03Hi I'm a new STM32 user . I'm wondering how to send data from the computer to the stm boardusing the RS232 cable .