STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! 4 line Nor flash speed during memory map mode

Hi I use STM32H743XI and W25Q256 for my design.And I notice W25Q256 has two speed 133Mhz(W25Q256JV) and 104Mhz(W25Q256FV), currently I use W25Q256FV, since I only use this flash with memory map mode, is it necessary to replace with W25Q256JV? Will th...

ZhouJianQiang_0-1729136629793.png ZhouJianQiang_1-1729136668450.png

STM32 for high speed ADC > 100 MSPS

Hi,My customer wants to design a high speed ADC aquisition system with minimum 100 MSPS rate and 14-bit resolution.The external ADC devices like AD9258 and AD9268 have this capability, which we are proposing.Would it be possible to use a high speed S...

Resolved! STM32 for live streaming

Hi,we would like to add live video playing/streaming to an STM32-based board we are designing that uses MIPI-DSI to drive a touch display, and we are at the stage of choosing the micro.Ideally it would stream from HDMI signal but we can use another i...

Ricko by Senior III
  • 3396 Views
  • 2 replies
  • 3 kudos

Resolved! H723Z external SD Ram clock no signal IS42S16400J-6TL

I'm working on a custom board with a STM32H723ZG. I'm also using external sd ram part  IS42S16400J-6TL found here (https://www.digikey.com/en/products/detail/issi-integrated-silicon-solution-inc/IS42S16400J-6TL/2708625). I've followed the excellent s...

fihes47572_0-1728664562680.png fihes47572_1-1728664583453.png fihes47572_2-1728664605152.png fihes47572_3-1728664611380.png

Resolved! Question about VREFBUF configure

Hi,I am using STM32H725REV6 chip in our product. Based on my understanding, since this is 68pin version which doesn't have VREF+ pin, the VREF+ is internally connected to VDDA. If my understanding is correct, I would like to ask if we would like to u...

EricZ by Associate
  • 1036 Views
  • 1 replies
  • 1 kudos

Resolved! STM32H735 ADC DMA Ethernet memory issue

HiI have implemented ADC1 on a DMA and verified its operation. I then implemented the ethernet stack and verified that it can be pinged. The issue I'm having is that the ADC DMA stops working once the ethernet stack is implemented. I believe the erro...

Resolved! DMA with multple variable

 I have three variables:volatile uint16_t a[20000];volatile uint16_t b[20000];volatile uint16_t c[20000]; However, I only have one DMA channel.Can I use the DMA to transfer these three variables together in circular mode?starting with the first 10,00...

xkamail by Associate II
  • 774 Views
  • 1 replies
  • 0 kudos

Resolved! IO port always readuing 0v in release mode.

Hi   I am using a STM32L433 and have a digital input pin, which is checked on bootup and enables the USB if 3.3v is in the pin.  When working in debug mode, it always works, but when I switch to release mode , using stm32CubeIDE , it always reads 0v,...

Resolved! GPIO Trouble on STM32 F767ZI

I used a Nucleo F767ZI dev board to check and write firmware(The IC on the board is STM32F767ZIT6U with the other characters being AA 254 VQ Z on first line and TWN AA 341 on line 2),when I use HSI clock I am able to operate PD7, PG9, PG10, PG11, PG1...