STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Reference power design for USB OTG host AND slave modes

Posted on March 08, 2012 at 16:35Hi Does ST have a reference design for an USB OTG use case where e.g STM32F4xx based board could be used both as a USB host providing 5V to the USB device and as a USB slave powering the whole board from the USB's 5v...

tuomas by Associate II
  • 1529 Views
  • 2 replies
  • 0 kudos

STM32VL with LCD

Posted on February 13, 2012 at 15:48Hello, Je suis un d�butant et j'essaye de commander une LCD (16 * 2) avec un STM32VL : afficher et ajuster une horloge (a l'aide des deux boutons B1 et B2 sur la carte) sur le LCD .et je sais pas par quoi je comme...

Troubles at receive more than one character (RTOS-RL-ARM)

Posted on March 02, 2012 at 12:34How to send and receive data using RTOS (RL-ARM) with tasks? (Without generating an interruption?) Using this functions below:TO SEND /*----------------------------------------------------------------------------   W...

esiqueira by Associate II
  • 1199 Views
  • 3 replies
  • 0 kudos

SWD Debugging multiple devices on one bus.

Posted on March 08, 2012 at 10:02According to this paper: http://www.arm.com/files/pdf/Low_Pin-Count_Debug_Interfaces_for_Multi-device_Systems.pdf, it is possible to use SWD to debug multiple chips that are all connected to the same debug lines. Acc...

mgerth by Associate
  • 1031 Views
  • 0 replies
  • 0 kudos

stm32f407 ADC data alignement problem -> solution

Posted on March 07, 2012 at 16:05I encountered a data alignement problem when using the 3 ADCs. ADC_Mode = ADC_TripleMode_RegSimult ADC_DataAlign = ADC_DataAlign_Right had no effect. Data was allways left-aligned. The Problem was that I omitted assi...

raffael by Associate II
  • 972 Views
  • 1 replies
  • 0 kudos

STM32F103xx Boundary Scan

Posted on March 07, 2012 at 15:21Hello, we use the STM32F103xx series for a long time now and want to know if it has boundary scan cells. Where can i find more information about the boundary scan possibilites of the microcontroller family of ST ? Fr...

duroyf by Associate
  • 808 Views
  • 0 replies
  • 0 kudos

CL1 & CL2 Value for Crystal (HSE)

Posted on February 29, 2012 at 16:49Hi, I have chosen this 25Mhz Crystal to be my next HSE:   http://at.farnell.com/abracon/abm8g-25-000mhz-18-d2-t/crystal-25mhz-18pf-smd/dp/1788523#similarProducts Datasheet: http://www.abracon.com/Resonators/ABM8G....

sam239955 by Associate II
  • 2768 Views
  • 7 replies
  • 0 kudos

USB Device (MSC): how to wait for data ?

Posted on March 06, 2012 at 05:20I'm trying  to implement USB device that emulates mass storage on USB FS, however, the data source  is approx. 10 times slower than USB FS transmit rate.I tried to wait in Mass Storage read callback for data, but it ...

dzuikov by Associate II
  • 1540 Views
  • 2 replies
  • 0 kudos