Skip to main content
frankfrank953
Associate II
May 12, 2010
Question

SPI2

  • May 12, 2010
  • 3 replies
  • 802 views
Posted on May 13, 2010 at 00:44

SPI2

    This topic has been closed for replies.

    3 replies

    smart2
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:50

    /* Defines for the SPI and GPIO pins used to drive the SPI Flash */

      #define SPI_FLASH                      SPI2

      #define SPI_FLASH_CLK             RCC_APB1Periph_SPI2

      #define SPI_FLASH_GPIO            GPIOB

      #define SPI_FLASH_GPIO_CLK        RCC_APB1Periph_SPI2

      #define SPI_FLASH_CS_GPIO_CLK     RCC_APB2Periph_GPIOB

      #define SPI_FLASH_CS                      GPIO_Pin_12

      #define SPI_FLASH_PIN_SCK         GPIO_Pin_13

      #define SPI_FLASH_PIN_MISO        GPIO_Pin_14

      #define SPI_FLASH_PIN_MOSI        GPIO_Pin_15

      #define SPI_FLASH_CS_GPIO          GPIOB

    /*******************************************************************************

    * Function Name  : SPI_FRAM_Init

    * Description    : Function to initialize SPI

    * Return         : None

    *******************************************************************************/

    VOID SPI_FRAM_Init(VOID)

    {

      SPI_InitTypeDef  SPI_InitStructure;

      GPIO_InitTypeDef GPIO_InitStructure;

      /* Enable SPI and GPIO clocks */

      RCC_APB1PeriphClockCmd(SPI_FLASH_CLK | SPI_FLASH_GPIO_CLK | SPI_FLASH_CS_GPIO_CLK, ENABLE);

      /* Configure SPI pins: SCK, MISO and MOSI */

      GPIO_InitStructure.GPIO_Pin = SPI_FLASH_PIN_SCK | SPI_FLASH_PIN_MISO | SPI_FLASH_PIN_MOSI;

      GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;

      GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

      GPIO_Init(SPI_FLASH_GPIO, &GPIO_InitStructure);

      /* Configure I/O for Flash Chip select */

      GPIO_InitStructure.GPIO_Pin = SPI_FLASH_CS;

      GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;

      GPIO_Init(SPI_FLASH_CS_GPIO, &GPIO_InitStructure);

      /* Deselect the FLASH: Chip Select high */

      SPI_FLASH_CS_HIGH();

      /* SPI configuration */

      SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;

      SPI_InitStructure.SPI_Mode = SPI_Mode_Master;

      SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;

      SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low;

      SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge;

      SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;

      SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_2; /* PCLK1 = HCLK/4  72/4=18= 18/2= 9Mhz*/

      SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;

      SPI_InitStructure.SPI_CRCPolynomial = 7;

      SPI_Init(SPI_FLASH, &SPI_InitStructure);

      /* Enable the SPI  */

      SPI_Cmd(SPI_FLASH, ENABLE);

    }

    frankfrank953
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:50

    Thanks guys. I spotted that about 20 minutes after posting .... I feel like such a muppet, I must stop working late as it all blurs together

    Tesla DeLorean
    Guru
    May 17, 2011
    Posted on May 17, 2011 at 13:50

    I am having a problem setting the RCC_APB2Periph_SPI2 because there is no define for the register value

    Because it is on the APB1 bus, not APB2

    RCC_APB1Periph_SPI2

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..