STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB Composite Device for DFU

Posted on May 18, 2012 at 14:37Hi everyone,I m trying to be in USB Mass storage Mode by default, and being able to do DFU action upload and download.I read that I have to disable all other interface to get in DFU mode.Thus, I wanted to use DFUSE to ...

gregoire by Associate II
  • 1262 Views
  • 1 replies
  • 0 kudos

DC32 Instruction

Posted on May 18, 2012 at 21:45 Hello -- We're trying to bring up FreeRTOS on our STM32F103c8 micro. In the function vPortStartFirstTask (file portasm.s) there is an SVC call as follows: cpsie i     0x8002efe: 0xb662         CPSIE     i  svc 0     0...

markbell9 by Associate II
  • 1787 Views
  • 1 replies
  • 0 kudos

problem with calculating internal tempwerature with STM32F105

Posted on May 16, 2012 at 23:26Hello I have a problem with calculating internal temperature with STM32. When processor VCC is 3.3V everything is ok - temperature is almoast accurate with wide temerature range. But whet processor VCC is below 3V temp...

wadi by Associate II
  • 1345 Views
  • 2 replies
  • 0 kudos

Using cortex-m4 FPU with gcc toolchain

Posted on May 16, 2012 at 06:43Dear all, I'm using `Keil uVision` with gcc toolchain (Sourcery Codebench lite for ARM EABI) to program the `STM32F4 cortex M4` chip. The compiler control strings I have set are:     -march=armv7e-m -mfpu=fpv4-sp-d16  ...

ID Unique device ID register (96 bits) “,

Posted on May 16, 2012 at 15:12Hello,  The Cortex M3 have the �ID Unique device ID register (96 bits) �, this number give to the user application technical information about the Cortex M3 mounted in the PCB ?. Extract from the datasheet RM008 revisi...

xgarcia by Associate
  • 1325 Views
  • 4 replies
  • 0 kudos

Difficuly of implementing nand driver on STM32F205ZG

Posted on May 15, 2012 at 08:47Hi all, Now, I'm trying to implement nand driver of  SAMSUNG K9K8G08U0D (SLC, 1GBYTE) on STM32F205ZG cpu. However, it not easy to do it. First, reading device ID is OK. Second, block erase function is also OK. But,...

kpkang by Associate
  • 2063 Views
  • 2 replies
  • 0 kudos

Need for Backup registers > 4KBytes

Posted on May 15, 2012 at 19:31I wonder if someone could help me. I need to save, to retain ''some'' variables of my applications, but the 4Kbytes from the Backup registers is too few for what I need. So I would like to ask if there is another way t...

tecnico23 by Associate II
  • 2169 Views
  • 12 replies
  • 0 kudos

Slope of internal temperature sensor

Posted on April 10, 2012 at 11:25Hello, we are using the microcontroller STM32F100C6T7 in our design. While trying to do something with the internal temperature sensor we noticed that the slope we measured doesn't correspond with the specified slope...

kbroger by Associate
  • 2071 Views
  • 4 replies
  • 0 kudos