STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32F205: 96 unique ID: use only 32

Posted on September 27, 2012 at 18:35Does anybody know if the 96bit unique-ID has different fields? There's no much info about this unique ID (in the reference manual it is said that it has 96bits but after that, when the register is shown only the ...

miriarte by Associate II
  • 1841 Views
  • 1 replies
  • 0 kudos

Break / PWM - STM32F4

Posted on September 27, 2012 at 10:41Hi Folks, I like to disable PWM, on an external event - i want to use BKIN. i set the break mechanism up like this ------......    GPIO_PinAFConfig(GPIOB, GPIO_PinSource12, GPIO_AF_TIM1);     /* Automatic Output ...

finnb2 by Associate II
  • 1570 Views
  • 3 replies
  • 0 kudos

Break / PWM - STM32F4

Posted on September 27, 2012 at 10:30Hi Folks, I like to disable PWM, on an external event - i want to use BKIN. i set the break mechanism up like this ------......    GPIO_PinAFConfig(GPIOB, GPIO_PinSource12, GPIO_AF_TIM1);     /* Automatic Output ...

finnb2 by Associate II
  • 1424 Views
  • 2 replies
  • 0 kudos

STM32 & Keil memory management in C++

Posted on September 27, 2012 at 09:12Hello, I am using Keil and I have started to try using C++. That seems to work okay except that i ran into some strange behaviour for which I have no explanation. Lets say that I have 4 different classes C1, C2, ...

longchair by Associate III
  • 1950 Views
  • 4 replies
  • 0 kudos

STM32F100 UART problem

Posted on September 25, 2012 at 09:06Hello,I'm currently trying to implement a UART driver with interrupt handling for the STM32F100x6 on my Discovery board. but I am unable to receive or send data and even the interrupts are not getting generated. ...

sumanth by Associate II
  • 2329 Views
  • 6 replies
  • 0 kudos

STM32F4 and LXI devices.

Posted on September 27, 2012 at 10:50Hi everybody, I'm working with a STM32F4 uC and I need to drive a LXI device. I'm searching for an example or a library to start. Anyone can help me? Thanks a lot and sorry for my english. #library #lxi #stm32...

tommaso by Associate II
  • 1082 Views
  • 0 replies
  • 0 kudos

counter clock PWM INPUT

Posted on September 20, 2012 at 01:55Hi every one Is anybody know how can i change counter clock i'm using PWM INPUT example this quote got from readme file: The TIMxCLK frequency is set to SystemCoreClock/4 (Hz), the Prescaler is 0 so the counter c...

imanpakii by Associate III
  • 1753 Views
  • 7 replies
  • 0 kudos

stm32f4discovery bootloader

Posted on August 31, 2012 at 15:23I have a porblem with the stm32f4 bootloader!The initialisation of the bootloader via USART1 (PA9/PA10) works so far.I am using a stm32f4discovery-board. The problem ist that it only works with very low baudrates. I...

mwolke9 by Associate II
  • 2531 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.