STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L Hard fault after waking up from EXTI

Posted on December 18, 2012 at 03:22I'm programming for an STM32L152xx and ran into the part hard faulting when it goes to sleep but wakes up from an external interrupt. Since I need the lower power sleep mode, I'm doing the necessary steps to get t...

shotaro by Associate II
  • 1474 Views
  • 2 replies
  • 0 kudos

STM32F100C4, TIM1 problem

Posted on December 16, 2012 at 20:19Hello! I've faced with next challenge: my STM32F100C4 freezes right after TIM1 interruption occurs. When I used simulator of Keil (this MCU isn't supported by simulator, so I specified STM32F103C8) I found place i...

STM32F105 USBD_FS_VCP

Posted on December 17, 2012 at 16:12hi  all, I have bought a STM32F105R8 demo board,   the board can communicate USART1 to CAN1.  now I want to try the USBD and CAN1 in FS mode, so I downloaded the “STM32_USB-Host-Device_Lib_V2.1.0â€� from http://...

evanqian by Associate II
  • 1673 Views
  • 3 replies
  • 0 kudos

. .

Posted on December 17, 2012 at 09:35 #i2c

ahiggins9 by Associate II
  • 2990 Views
  • 7 replies
  • 0 kudos

GPIO pull - up/down configuration

Posted on December 17, 2012 at 11:17Hi All,CNF1 and CNF0 bits at port configuration register. 11 is reserved , 10 makes it pull - up/ down.I think it connects pull up and down resistor at same time.Is it possible to select pull - up only.Thanks

akinik by Associate
  • 1583 Views
  • 3 replies
  • 0 kudos

Programming problem on Open407I-C with LCD

Posted on December 17, 2012 at 22:26I just started with the STM32F407 Open407I-C board:http://www.wvshare.com/product/Open407I-C-Standard.htmIt's a pretty excellent demo board.  Very little pin commitment on the board, most are just straight brought...

dannym by Associate III
  • 1368 Views
  • 2 replies
  • 0 kudos

Modyfing/replacing C funtion during STM32 work

Posted on December 17, 2012 at 14:48I'd like to implement simple DSP job on my STM32F4 discovery board. I wish to have possibility to change it during STM32 work without flashing program memory. Can I do that? It's like I compile some C funtion to m...

stm32 + gcc compiler

Posted on December 09, 2012 at 15:22Hi All, I have the stm3240g-eval board,currently i am working with keil uvision as my IDE + armcc,but i am willing to switch to gcc . My question is ,does anyone have a explantion on how to configure the Eclipse t...

USB CDC Device hung fix

Posted on August 16, 2012 at 20:52 Hello! Looks like there is a subtle bug in the USB CDC device implementation. I played recently with STM32F4DISCOVERY board. In order to test USB operation in VCP mode I've created simple code which just echo ev...

olegv by Associate
  • 2223 Views
  • 3 replies
  • 0 kudos

USBD_Init Arguments

Posted on December 14, 2012 at 21:39Hello :)I'm trying to programm a virtual com port with the stm32f4discovery.In the official document of STM called ''STM32F105xx,... USBOn-The-Go host and device library'' there are the following arguments for USB...