STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Clearing the OCxREF signal on an external event

Posted on February 14, 2013 at 14:30Hello.As described on STM32F100 manual:The OCxREF signal for a given channel can be driven Low by applying a High level to the ETRF input (OCxCE enable bit of the corresponding TIMx_CCMRx register set to ‘1’)....

casainho by Associate II
  • 3186 Views
  • 6 replies
  • 0 kudos

measure the duration of a loop ?

Posted on February 22, 2013 at 11:20Hi Can I measure the duration of a loop in the program of STM32F4 using TIMER ? For example ______________________________________ Begin (Timer x) For (;;) //infinite loop { .... ... ... .. } End (Timer x) ...

bmwael1 by Associate II
  • 2242 Views
  • 5 replies
  • 0 kudos

TIM14 @ STM32F103VGT6

Posted on February 22, 2013 at 18:10Hi, I would like to use TIM14 @ STM32F103VGT6 uC but it doesn't defined everywhere. Did anybody used this timer before? What was the startup file used? Best regards, #stm32-tim14-stm32f103vgt6

gsilva by Associate II
  • 1494 Views
  • 2 replies
  • 0 kudos

STM32F103RBT6 development board + 2.8'' TFT-module

Posted on June 25, 2011 at 19:59Hey people, Recently I bought the STM32F103RBT6 development board + 2.8'' TFT-module. (A.k.a MINI-STM32-V3.0) (with the 2 mini USBs) After many attempts to enter programming mode, and program it via USB without any ...

UART initialisation

Posted on February 22, 2013 at 09:24Hi everybody,I'm using a STM32F205VE and something that I don't understand.I do this :  USART_InitStructure.USART_BaudRate = 9600;  USART_InitStructure.USART_WordLength = USART_WordLength_8b;  USART_InitStructure....

STM32 CAN Receive Mailbox

Posted on February 20, 2013 at 13:40Hi,I am working with STM32F101 using CAN1 controller.I configure the CAN filter to accept messages from 0x100 to 0x1FF as follows:CAN_FilterInitTypeDef CAN_FilterInitStructure ; CAN_FilterInitStructure. CAN_Filte...

Stmf4-discovery debugger + USART problem

Posted on February 15, 2013 at 05:12I 'm new to stmf4 discovery and am facing problems in getting USART working on my STMf4 discovery board, I tried the same code as posted in the discussion ''F4discovery using Uart 1''. but when I click on ''make a...

GPIO Pull Up during reset.

Posted on February 20, 2013 at 12:38Hi everyone! I connected one STM32F103 GPIO pin configured as OutputPP to -> a STM32F0 GPIO pin configured as Input Floating with EXTI. While STM32F103 hardware reset, the line is pulled down, so the STM32F0 EXTI ...

franmoya by Associate
  • 1891 Views
  • 2 replies
  • 0 kudos

worst forum software ever

Posted on February 22, 2013 at 11:08In Fabrice's previous post, until ''Show Quoted Messages'' is clicked, part of the code (the first 10 lines or so) are hidden. I hoped the remake of ST's web meant they already have fired the webmaster as they sho...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.