STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with printf on F0

Posted on March 07, 2013 at 20:21Hello, I have project in Keil for demonstrating USART on STM32F0.Program is working fine with putc, but with printf it isn´t working (building of program finish success in both case). Why printf isn´t work? My main...

hospodar by Associate III
  • 750 Views
  • 2 replies
  • 0 kudos

SPI on STM32F4

Posted on March 07, 2013 at 03:41Hello,       migrating from STM32F1xx to STM32F407. Having difficulties configuring 4-wire serial, sub-optimal documentation for the F4 series, in my opinion. There's a nice section in the reference manual for the F1...

0690X000006053iQAA.png

Issues with SPI 2 on STM32f100RB

Posted on March 07, 2013 at 17:02 I will need to use spi with a memory chip. But I currently can't get my spi to input data. I am able to get it to output. I have a logic analyzer hooked up and it shows data is being outputed. When I do a loop ...

kaylee by Associate II
  • 1168 Views
  • 2 replies
  • 0 kudos

fsmc and usart3

Posted on February 01, 2013 at 15:27i'm using stm32F103zc using its fsmc 8 bit mode and usart3 (PD8 PD9), can this design work ok? thanks

Using Bootloader Via USB With STM32F4

Posted on March 06, 2013 at 23:17I am trying to establish a connection with the bootloader via USB using our prototype which has an STM32F407. I know the USB FS connection works because our firmware uses it to connect to the PC. Also, I can get the ...

ryanrj by Associate
  • 885 Views
  • 0 replies
  • 0 kudos

usart + sd card interaction

Posted on March 05, 2013 at 14:36Hi, I am using STM3240G-Eval , i know that in this evaluation board MicroSD Card shares I/Os with motor control, RS-232 and audio . So i am trying to work around this limitation. I have the following flow : initUSART...

stm32f4 discovery and dac

Posted on March 05, 2013 at 14:19hey there,recently I've started playing with a stm32f4discovery with the final goal of realizing the control of a particular simple device we had in our company. It is my first embedded project so I'm quite new to th...

multi ADC and DMA ==> memory problem

Posted on March 05, 2013 at 16:57Hello, I need to measure 3 ADC channels in continuous, I use the STM32L151VB. I use the DMA transfert, my firmware doesn't work property. please see in attachment my source code my problem is the  memory data  ''adcB...

willdu87 by Associate
  • 1168 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.