STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DMA for unknown datareceive throw USART

Posted on March 18, 2013 at 15:24Hello, I am working on a device which one funcion should be USART to Ethernet bridge on STM32F407. I need to receive data from USART and then work with them. But beacuse of speed I wanted to use DMA instead of interr...

phajek by Associate
  • 2103 Views
  • 4 replies
  • 0 kudos

STM32F103C6 Increase flash page erase time with IWDG active

Posted on February 28, 2013 at 11:58Hi, I've noticed an extra time in the erase page process when the IWDG is active. I haven't measured it (I notice a change in the blinking frequency of a led) and it's not a big deal, but I can't find any referenc...

xbalmes by Associate II
  • 3387 Views
  • 9 replies
  • 0 kudos

STM32L-DEV (STM32L152RBT6) + I2C with interrupts

Posted on March 17, 2013 at 20:42Hello,I'm new in ST micro controllers. I'm trying to write I2C application that sends and receives data with interrupts, but I can't find information about it.May be anybody knows where to find examples of code of it...

STM32F10x_DSP_Lib_V2.0.0 where to find?

Posted on March 17, 2013 at 20:17Hi All! I just start with stm32 exacly with STM32F103VBT6, i have evaluation kit and i need library named: STM32F10x_DSP_Lib_V2.0.0 and sd_stm32.c where i may find it? Thanks for You patience! #lmgtfy

STM32 USART DR unavailable

Posted on March 14, 2013 at 09:35 Hey, guys! I have one stupid error, show me the right way, please. I'm actually working with STM32L-Discovery and trying firstly to work out the USART. I've done all necessary configurations for th...

dima by Associate II
  • 3438 Views
  • 6 replies
  • 1 kudos

STM32F4 RTC and LSI question

Posted on March 17, 2013 at 15:31Hi I'm just wondering why the LSI on the STM32F4 Discovery board has inaccuracy's, I've searched the internet and application notes but can't seem to find the answer? My seconds on LCD jumps several times between 0-6...

bee2 by Associate II
  • 1896 Views
  • 4 replies
  • 0 kudos

low power mode (snapshot) on OV2640

Posted on March 17, 2013 at 17:37I'm working on a project where power consumption is a critical issue. I need to store a frame from a camera (OV2640) on the uSD each 2 seconds. My problem is that the camera's clock is always on which bring the power...

problem with generation of sine wave

Posted on March 09, 2013 at 14:29Hello, I am trying to generate sinusoid signal via DAC. I can´t use look up table of sine values, because user will enter amplitude. So values of sine are first computed in program and than stored in buffer: sine[i...

j3lda by Associate II
  • 1742 Views
  • 4 replies
  • 0 kudos

STM32F & 4-quadrant complementary switching

Posted on March 16, 2013 at 21:38Hello, I want to implement the bipolar 4-quadrant complementary switching using STM32F103C8 TIMER1. The bipolar switching requires that the top and bottom switch PWM signals need to be swapped.I have read STM32F103C...

STM32F407 I2S High speed trouble

Posted on March 09, 2013 at 17:28 Hello peolpes, maybe somebody can help me. For a testing I use two I2S - one(I2S3) for transmitting, second (I2S2) - for receiving, phisicaly connected at the PCB. At both I use Double Buffer DMA...

alexandr by Associate II
  • 4452 Views
  • 14 replies
  • 0 kudos