STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Java binary

Posted on May 07, 2013 at 16:41Hi,Resulting  binary can be downloaded to a general STM32  or only to a Java enabled one?

5V & 3V3 POWER SUPPLY BAT60 DIODES: are they critical ?

Posted on May 20, 2013 at 12:11Hello,I'm currently designing my own schematic based on the STM32F4DISCOVERY board.The two BAT60 power supply protection diodes (D1 & D3) are not relevant for me because they generate a dropout voltage: +5V is in fact ...

STM32F4 with external NAND-Flash - whats the Adress Area?

Posted on May 28, 2013 at 01:00Hi, I'm using this Board: http://www.keil.com/support/man/docs/mcbstm32f200/mcbstm32f200_to_memory.htm to build up a small webserver interface. I want to put the website data on the NAND-Flash. But what is the Adress o...

sam239955 by Associate II
  • 1194 Views
  • 1 replies
  • 0 kudos

adding USB interface descriptor

Posted on May 26, 2013 at 19:53The original post was too long to process during our migration. Please click on the attachment to read the original post.

stm32 by Associate
  • 1125 Views
  • 1 replies
  • 0 kudos

USART1 with missing bytes

Posted on May 27, 2013 at 06:21 I am trying for now to send 600 001 bytes to PC from stm32f4 discovery board. below is how USART configured: uint32_t config_usart3( void ) { //===========================================================...

Including startup into library

Posted on May 27, 2013 at 16:45Hello,I need to create a library to my BSP so I would be able to use it anywhere.Creating the .a file isnt that hard with CooCox IDE, but the main problem is when I want to use the library in an application, the size o...

bouhoula by Associate II
  • 1160 Views
  • 2 replies
  • 0 kudos

DMA to USART1 TX

Posted on May 27, 2013 at 13:17Hi, i'm using smt32F303 discovery board, I send / receive data on USART1 without problem if I use interrupt mode, so I think that hardware is good.I want send a data buffer lenght ~ 8000 bytes using dma mode. Before I ...