STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

AN3070 : Is DMA transfer complete interrupt needed?

Posted on May 27, 2013 at 05:31Application note AN3070 describes a procedure for releasing RS485 bus when using DMA to transfer USART data.   The procedure uses two interrupts:  * DMA transfer complete (DMA_TC) interrupt   * USART transfer complete ...

derek by Associate II
  • 1653 Views
  • 2 replies
  • 0 kudos

unable to get into bootloader on stm32f103

Posted on May 31, 2013 at 08:59Hi, i bought 2 chips STM32F103RET6 , i put them into boards, one chip is working normally , so it's possible to flash it via USART1, but second one is not reacting on USART1 for new flash, and i think that it's not ...

Problems blinking blue LED

Posted on May 31, 2013 at 14:53Hi all! I'm a newbie and I have problems with my STM32L-Discovery. I'm trying to do the simplest possible program: make the blue LED in PB6 output blink. This is the code I've made: #include <stdio.h>                  ...

STM32F407VGT6 + Kamera (OV7670) + Ethernet Stream

Posted on May 31, 2013 at 10:03Hello, I currently have the problem of the camera (OV7670) via Ethernet (UDP) to stream. I currently use the demo software and a simple UDP connection (server) to build, now I want to send the camera data in JPEG form...

samet by Associate
  • 1095 Views
  • 1 replies
  • 0 kudos

decibel - microphone - st32f4 discorvery board

Posted on May 27, 2013 at 16:50 I test the microphone[MP45DT02] of stm32f4 discorvery board.    I use 1.024Mhz Clock input microphone with i2s signal. Pmd fiter of  library is applied and get pcm data from pdm data. Is it corret pcm data that no sou...

sojaewoo by Associate II
  • 2605 Views
  • 6 replies
  • 0 kudos

STM32L1 STOP MODE

Posted on May 30, 2013 at 16:21Hi,Stm32l1 consumes much current than I expected. In standby mode, I measure 6uA consumption for my board but when I put it in stop mode it consumes 480uA. It should be around 10uA.The configuration is; USART_ITConfig(...

hs / fs usb, discovery f4

Posted on May 30, 2013 at 12:28Hi, I believe that FS is USB1 and HS is USB2. I have FS running in my project but can't seem to get HS running.I can run this ST sample on the f4 discovery board: http://www.st.com/web/en/catalog/tools/PF257882I have t...

ian239955 by Associate II
  • 2750 Views
  • 7 replies
  • 0 kudos