STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4xx __disable_irq(void)

Posted on July 01, 2013 at 15:36 Writing in 'C', I use __disable_irq(void) before reading a value that gets updated in an interrupt service routine. __disable_irq(); //prevent serial interrupts Count = TSp->DataAvailable; //get number...

John F. by Senior
  • 2869 Views
  • 6 replies
  • 0 kudos

STM32F333?

Posted on June 03, 2013 at 23:11When willthesaleSTM32F333, of which are  referred  in http://www.arroweurope.com/nc/services/downloadcenter.html?tx_abdownloads_pi1%5baction%5d=getviewclickeddownload&tx_abdownloads_pi1%5buid%5d=868&tx_abdownloads_pi1...

asrock70 by Associate II
  • 1592 Views
  • 3 replies
  • 0 kudos

STM32F10C-Eval ethernet connector

Posted on July 01, 2013 at 10:41Hi, I connected the ethernet port of the STM32F10C-Eval with the Hub using an ethernet cable. But the ethernet port is not detected. What  could be wrong? Thank you.

IAR EWARM project doesn't run with STM32 startup file

Posted on July 01, 2013 at 18:05I'm attempting to test out some basic programs on an STM32L151RD (Cortex-M3) using IAR's Embedded Workbench. I'm using an ST-LINK/V2 programmer. I've downloaded the Standard Peripherals Library and generally have been...

amayberr by Associate
  • 1963 Views
  • 1 replies
  • 0 kudos

Imprecise bus fault

Posted on June 27, 2013 at 17:48I have recently run into a imprecise bus fault problem as indicated by my hard fault handler. I am using an Olimex STM-P103 development board (STM32F103RB CPU) and there is no OS or RTX present. I am pretty certain th...

dsjnews by Associate III
  • 3876 Views
  • 6 replies
  • 0 kudos

STMStudio 3.1.1 does not show all variables on import

Posted on March 13, 2013 at 11:57Hi, after I updated the STMStudio I'm not able to import all variables from the .efl file. After selecting a file there are not all variables shown. I tried different toolchains, but the problem is still there. I use...

STM 32 Debug Mode

Posted on July 01, 2013 at 06:48Dear All,                 I am new to this STM microcontroller. I started working on with some of the few examples provided in keil 4 .Presently i am working on STM32F217IG controller for which I wrote a small program...

How start running STM32 firmware from IROM2 ?

Posted on July 01, 2013 at 06:27I'm developing an embedded application using Keil MicroVision 4 & STM32F103RE I've splited Flash memory of device into two areas (IROM1 & IROM2) using IDE target options panel (Target tab, Read only memory areas secti...

MAC Address in Memory

Posted on June 30, 2013 at 08:57Hello, Where is the best place in memory to keep the MAC Address in STM32F207? It should not be changed with FW updateds. Yuval #stm32f207-mac-address

yuvalk by Associate II
  • 1366 Views
  • 2 replies
  • 0 kudos

SDIO DMA Timeout

Posted on June 24, 2013 at 15:13 Hi All , Till now i worked with the STM3240G-EVAL , At the beginning i had a problem that i received DMA timeout when i tried to write to the sd-card. The was due to a problem that the DMA interrupt ,...