STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

The 32bit@32cents : STM32F030 Value Line

Posted on July 08, 2013 at 16:03STMicroelectronics has announced today in Bangalore the STM32F030 Value Line : the 32bit@32cents :)The STM32F030 features an ARM Cortex M0 core and runs at speedsup to 48 MHz like other today members of STM32F0 Series...

DCMI DR (data register) problem

Posted on July 08, 2013 at 07:49Good day,I have some problems with uint32_t DCMI_ReadData(void); function.I always have 0 data from that DCMI->DR register.I use STM32F4DISCOVERY board, (stm32f407vgt6 MCU).My interupt handler:void DCMI_IRQHandler(voi...

hitsumen by Associate II
  • 709 Views
  • 1 replies
  • 0 kudos

can i debug stm32 with stm-studio and MDK together?

Posted on July 04, 2013 at 15:04Can i debug stm32 with stm-studio and MDK together? I found that stm-studio and MDK can not debug stm32 at the same time. The reason is ST-LINK(v2) can not be connected by MDK and STMStudio at the same time.  #stm3...

STM32F103 I2C interrupt driven method 2

Posted on January 16, 2012 at 22:29I am having issues with interrupt driven I2C using method 2 from the reference manual. I am trying to read from the magnetometer on an lsm303dlh. The least significant bit of the most significant byte seems to be t...

eexlb2 by Associate
  • 2650 Views
  • 3 replies
  • 0 kudos

STM32F103 HD - Initial Stack Pointer is Wrong

Posted on July 07, 2013 at 18:55I'm trying to set up a project (Eclipse, gcc, OpenOCD) for a hand made prototype board using an STM32F103RC chip (48K RAM).  It works, sort of.  My linker script specifies the initial stack pointer as _estack = 0x200...

SPINFamily Evaluation Tool + STEVAL-PCC009V2 + EVAL6480H R1.1

Posted on May 14, 2013 at 19:05Hello,I want to get the SPINFamily Evaluation Tool (L6480) working but everytime I get an error message to make sure the communication board (STEVAL-PCC009V2) is connected to the PC and board firmware has been updated ...

loibl2 by Associate II
  • 4648 Views
  • 6 replies
  • 0 kudos

STM32f2xx could not work with maximum frequency

Posted on July 03, 2013 at 13:27I'm using default configuration (according to UM1061, RCC section) to configure an SMT32F215RG to work with 120MHZ CPU clock. here is my configurations: /* PLL_VCO = (HSE_VALUE or HSI_VALUE / PLL_M) * PLL_N */ #define...

PWM Output

Posted on July 05, 2013 at 13:25The original post was too long to process during our migration. Please click on the attachment to read the original post.

andykim by Associate II
  • 948 Views
  • 2 replies
  • 0 kudos

Max232 level shifter

Posted on July 05, 2013 at 12:02hello i have usb <-> R232 converter and i want to make it receive correct characters from stm32f4 board , so which capacitors i have to use with max232 to realise this ? and thnx :)