STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H750IBT6 Bootloader Problem

Hello everyone. I am trying to write a bootloader with STM32H750IBT6 and mt25ql512. I am trying to adapt the ExtMem_Boot example of STM32H750-DK to STM32H750IBT6 by modifying it, but I can't succeed. It doesn't make sense why STM32H750IBT6 does not w...

MKoca1_0-1729669938505.png
MKoca.1 by Senior
  • 3538 Views
  • 9 replies
  • 2 kudos

Supported PSRAM and Flash for the STM32N6xx

Hey guys, I'm looking for some suitable HexaSPI PSRAM and also the OctoSPI Flash for the STM32N645 board I am just building.. I cant find the parts used on the DK so do you have a list of supported memories? I need 256Mb PSRAM and will start with a 1...

RAdam.1 by Associate III
  • 757 Views
  • 5 replies
  • 4 kudos

Resolved! STM32G474RET6 VREF connection

Hello, I am planning to use the STM32G474RET6 and would like to confirm whether I can use the internal VREFBUF. This product's package is LQFP-64 and while reading the datasheet I noticed the note : ''The VREF+ pin is double-bonded with VDDA on some ...

Resolved! STM32H573 - missing BKPSRAM on memory map

Hello,The datasheet and reference manual are missing information about the 4 KB Backup SRAM in the memory map.Where can I find details about it?We need to use this memory in both Secure and Non-Secure projects.Thank you. 

RZub by Associate II
  • 252 Views
  • 3 replies
  • 1 kudos

Resolved! FDCAN not receive messages from a few particular sensors

Dear allI am using STM32H563 and interface with some CAN bus sensors to receive and sometimes send data to them. The CAN bus sensors are developed by a partner company. I developed my software refer to FDCAN_Com_IT example provided in IDE firmware pa...

Ping1 by Associate II
  • 484 Views
  • 10 replies
  • 1 kudos

Resolved! STM32L4 STOP2 System abnormal restart

Environment: STM32L4 + 32.768K LSEFunction: Wake up and work once every hour, then enter stop2 mode. During the one-hour sleep, wake up every ten minutes to feed the external watchdog.Problem: The device resets directly when waking up every ten minut...

daniaoday by Associate III
  • 2019 Views
  • 54 replies
  • 8 kudos

Stm32h743 gets hot on custom PCB

I designed a PCB using the STM32H743 in the TFBGA240 +25 package.When I power the board, the STM32 gets hot. I measured the voltage across the VCAP capacitors, and it is 2.2 V, while it should be a maximum of 1.35 V.What could be causing the VCAP vol...

Resolved! reset_handler and no longer debug

Hello, I was writing some code and one day a handler_reset() appears in the debug panel It is said that appears because it give the opportunity to the user to debug from the very begining. But why? if there is already the ability to set the breakpoin...

carleslsregner_0-1770115368451.png carleslsregner_1-1770115965402.png carleslsregner_2-1770115997060.png