STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f4 interrupt pipeline hazard

Posted on October 21, 2013 at 10:26 Hello again, I have learned that this: void DMA2_Stream3_IRQHandler() { // Test if DMA Stream Transfer Complete interrupt if (DMA_GetITStatus(DMA2_Stream3, DMA_IT_TCIF3)) { DMA_ClearITPend...

mail2 by Associate II
  • 4775 Views
  • 3 replies
  • 0 kudos

Frequency Capture

Posted on June 08, 2013 at 12:03I am using stm32f103rbt6 for frequency capturing. I am trying to use timer1 channel1 and channel2 to capture two different frequency say 1K and 500 hertz. Once 1k frequency rising edge is detected i am reading the CCM...

aru by Associate II
  • 1557 Views
  • 3 replies
  • 0 kudos

DMA and ADC on the STM32F2xx

Posted on October 18, 2013 at 22:41Trying to stuff multiple channels of ADC3 into a DMA, but am unsure of how the DMA address gets incremented. Is this done automatically behind the scenes and I don't have to worry, or am I missing a setup?  I didn'...

how to check DMA ISR source within a channel

Posted on October 18, 2013 at 10:21Say on my device, in DMA ch1  i can have 3 periphs, plus possibly mem2mem. If I installed an isr how do I check from which periph (or mem) it came from, by reading  DMA_CPARx PA bits ?  #dma

denis by Associate II
  • 3016 Views
  • 8 replies
  • 0 kudos

STM32F4 CAN data problem

Posted on July 09, 2013 at 08:49 Hi all, I am using the CAN interface on the STM3240G-EVAL for a CanOpen implementation. All works fine up until the point where I need to transfer data via CanOpen PDOs which are more than 6 bytes in le...

hermanv by Associate II
  • 4656 Views
  • 9 replies
  • 0 kudos

Problem with DMA on USART1 on STM32F0xx

Posted on October 19, 2013 at 19:42 Hi, I cannot get DMA receiver on USART1 to working state. I'm attaching code and would be thankful for any help or advice. Are there anywhere some working examples with DMA? I must be missing somet...

STM32f4 3.2'' ssd1289 tft orientation...

Posted on December 18, 2012 at 20:55Hi all & seasons greetin's.I have been using the HY32D 3.2'' TFT from China with the SSD1289.c and SSD1289.h library which I have had some nice results with thanks to MegaHercas.:)I was wondering if anyone has any...

sts0340 by Associate II
  • 2728 Views
  • 7 replies
  • 0 kudos