STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Suggested IDE

Posted on December 10, 2013 at 11:15Hi, I've been using MikroElektronika as my IDE for the last couple of months but am now at the stage where I'm growing very frustrated with it's bugs and issues. Was wondering what others are using and what you wo...

How is STM32F303 differential ADC input centered?

Posted on January 03, 2014 at 22:45I have been unable to determine from the datasheets or application notes what the real behavior of the ADC in the STM32F303 is when in differential mode.  This leads to two questions: 1) Can V_neg be greater than V...

aaron by Associate II
  • 2468 Views
  • 4 replies
  • 0 kudos

Problem with external interrupts

Posted on January 05, 2014 at 08:17I am trying to attach interrupt to my motor encoder ( connected to pin PB9). My idea is to get the pulse count as the motor rotates. Shown below is a snippet of my code to attach interrupt to pin PB9. I should be g...

Put HSE on MCO1

Posted on December 19, 2013 at 15:46 I have this code that is trying to put my HSE clock onto MCO1 (A8) on my STM32F407 Discovery, but it doesn't work. Anyone know what's wrong? #include ''stm32f4xx_gpio.h'' #include ''stm32f4xx_rcc.h...

USART to printf

Posted on September 29, 2010 at 21:18 @page {margin:2cm;} .ExternalClassB84147A5E35D4D54A6663AEC4519B806 P {margin-bottom:0.21cm;} I can compile and download the attach project to the STM32VLDISCOVERY without any warnings or errors. The code is...

finsprit by Associate
  • 2682 Views
  • 7 replies
  • 0 kudos

LCD Settings on STM32F429I-Disco

Posted on December 23, 2013 at 10:51Hello together,I try to get to work the STM32F4-Discovery-Board with the LCD-Display. I have the code of the graphic-workshop from ST. In this code the STemWin-Library of segger is used without the source code, on...

How can I add a new task on FreeRTOS on STM32 ?

Posted on January 06, 2014 at 06:32Guys, How can I add a new task on FreeRTOS on STM32 ? I have created : [CODE] #define LCD_TASK_STACK_SIZE            ( configMINIMAL_STACK_SIZE ) #define LCD_TASK_PRIORITY            ( tskIDLE_PRIORITY + 1 ) #defin...

Maximum Transfer Rate - USB Mass Storage STM32F103 SPI

Posted on January 06, 2014 at 02:10Hi,I am working on a couple of projects that incorporate USB Mass Storage, i am using an STM32F103RB MCU and the micro SD card is connected via SPI.The maximum transfer rate i am getting is around 85 kB/sec.I am tr...

STM32F4-Discovery Updated Libraries w/Makefiles.

Posted on January 06, 2014 at 02:24Problem: The STM32F4-Discovery samples haven't been updated in a long time and there aren't any free IDE or toolchains supported. As a brand new developer for STM coming from Arduino land this was rather difficult ...

st239955 by Associate II
  • 1721 Views
  • 1 replies
  • 0 kudos