STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Program doesn't run with Debug detached

Posted on January 16, 2014 at 16:40I have a STM32F415VG which I have on my own board. The program code all runs when I have my SW debug adapter hooked up, but if I try to run the program without the adapter connected, nothing works. My oscillator do...

TIM flags automatically set when TIM enabled

Posted on June 19, 2013 at 16:16Hello, I am facing a problem with the timers I am using in STM32f100 MCU. I have configured different timers to operate during the execution of the code, but somehow, all the flags related to Capture/compare or Update...

0690X00000602kvQAA.jpg
rachit by Associate
  • 1124 Views
  • 2 replies
  • 0 kudos

STM32107 Default Clock configuration

Posted on January 19, 2014 at 07:54I am trying to figure out the default clock speeds (after reset) for the buses and the peripherals and system clock for the STM32107VC. I am reading the STM32107 Reference Manual RM0008 on page 123.One thing I do n...

orlcp440 by Associate II
  • 2932 Views
  • 6 replies
  • 0 kudos

Changing EXTI lines

Posted on January 18, 2014 at 20:49 Hello, first I am sorry if I didn't need to open new thread. I searched through lot of examples in this forum, about EXTI. And most of them were similar to my problem, but non of them helped. :(<br>I am using ...

STM32F429I-discovery SPI Troubles

Posted on January 12, 2014 at 07:43 Hi, I just received my STM32F429 discovery board and I tried to implement basic SPI but I'm stumped as to why the logic analyzer output was different. Can anybody point out were I was wrong. Here is the code. ...

0690X00000605WkQAI.png
shan_rei by Associate II
  • 2982 Views
  • 5 replies
  • 0 kudos

Hard fault test

Posted on January 17, 2014 at 18:09In order to test the Hard Fault interrupt, I modified the Systick example on ''STM32F0xx_Discovery_FW_V1.0.0'' as follows.. on main.c I added two lines: ------------------------------ int main(void) { uint8_t* Byte...