STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Timer for stm32 discovery board

Posted on August 30, 2012 at 19:44Hello everyone, I am new to embedded programming. I was trying to make a simple program that measures frequency and ON time of two different i/p pulses. The frequency that I want to measure is in the range of 37 to ...

ss882 by Associate II
  • 2611 Views
  • 7 replies
  • 0 kudos

Question about USART??

Posted on February 21, 2014 at 16:17PLz can some one tell me why we must ''&'' the received value with 0x7F!!!!!!

elaroussi by Associate II
  • 1427 Views
  • 3 replies
  • 0 kudos

stm32f429

Posted on February 12, 2014 at 07:20i've got a little problem with my boarda pin is shorted to the ground, only this input is shorted to the ground.also shorting Idd pins, is shorting the supply power supply circuit and ldo going crazy hotim thinkin...

kostas by Associate II
  • 2746 Views
  • 8 replies
  • 0 kudos

HSI Accuracy on the Value line STM32L

Posted on February 21, 2014 at 15:26Hello,The following question I have applied to the support team,on yet another forum and still awaiting an answer. Once I get an answer,I will share it here.The Value Line series STM32L datasheet claims the HSI ac...

elil by Associate III
  • 1315 Views
  • 1 replies
  • 1 kudos

Problem in using TIM2 Flag Polling

Posted on March 02, 2013 at 17:22Hello, I want to use Timer2 to generate approx 1secs Pulse without interrupt. I want the code to sit in an endless loop while testing the TIM2 update interrupt flag or TIM2 CCP1 Flag (I plan to use Compare instead of...

Input capture STM32F429 Discovery

Posted on February 21, 2014 at 12:30 Hi, I have a problem with F429 Discovery board. I use PB4 (is a free pin) for input capture This the configuration: void TIM_Config(void) { GPIO_InitTypeDef GPIO_InitStructure; NVIC_Ini...

STM32L1 strange ADC reading

Posted on February 21, 2014 at 10:14Hi, please I need a little help.I'm using a STM32L151RCT6A in a project. We need to distiguish the hardware version of boards, so to use a single pin, we read the voltage on a partitor made of two resistor.It is c...

giuseppe by Associate II
  • 3119 Views
  • 7 replies
  • 0 kudos

STM32F205: Erasing FLASH sector by sector

Posted on February 17, 2014 at 15:12I am using STM32F205 and I have designed my own bootloader. Before FLASH programming, my bootloader always erase whole FLASH from sector 1 to sector 11 (it uses fixed count cycle through sectors without determinin...

petrovsky by Associate II
  • 1876 Views
  • 4 replies
  • 0 kudos